<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IrDA in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066541#M8626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I kind of gotten it working.&amp;nbsp; &amp;nbsp;IrDA being half duplex helps a lot if Rx or Tx one of them should be inverted so they fight less.&amp;nbsp; The baud rate still only works at 9600 when set to 32 OSR.&amp;nbsp; The pulses are all measured correctly. It gets data, but is wrong and fails my CRC check when I choose the wrong CRC.&amp;nbsp; The autobaud code in the FSL code is mildly wrong, as it trucates decimal points in the math in casting as Ints, but that didn't solve the problem either.&amp;nbsp; For now I'll just force OSR of 32 for 9600.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Aug 2020 12:30:31 GMT</pubDate>
    <dc:creator>sjones1</dc:creator>
    <dc:date>2020-08-04T12:30:31Z</dc:date>
    <item>
      <title>IrDA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066537#M8622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having issues getting my IrDA communications working on a 1064.&amp;nbsp; It appears to only get locked when I over-ride the autobaud to OSR 32 no matter the baud rate and it's accuracy (still &amp;lt;3%).&amp;nbsp; Does the silicon compensate the OSR for the smaller puls widths or is that the need of the 32 OSR?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 19:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066537#M8622</guid>
      <dc:creator>sjones1</dc:creator>
      <dc:date>2020-07-06T19:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: IrDA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066538#M8623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Infrared interface of LPUART module covers data rates only&amp;nbsp;between 2.4 kbits/s and 115.2 kbits/s.&lt;/P&gt;&lt;P&gt;There with four options of configurable transmitter narrow pulse:&amp;nbsp;1/OSR, 2/OSR, 3/OSR or 4/OSR narrow pulse when IR is enabled.&amp;nbsp;Common pulse widths are 3/16, 1/16, 1/32 or 1/4 of the bit length. These can be configured by selecting the appropriate oversample ratio and pulse width.&lt;/P&gt;&lt;P&gt;For example: Set narrow pulse width equal 3/16, the OSR need be 16 and TNP set to 3/OSR.&lt;/P&gt;&lt;P&gt;TNP bits at&amp;nbsp;LPUART Modem IrDA Register (MODIR)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2020 02:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066538#M8623</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2020-07-07T02:23:10Z</dc:date>
    </item>
    <item>
      <title>Re: IrDA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066539#M8624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's for transmit, my question was referring to the receive end more.&amp;nbsp; I get bad data unless I force OSR of 32 on buad 9600 and 115,200.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2020 12:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066539#M8624</guid>
      <dc:creator>sjones1</dc:creator>
      <dc:date>2020-07-07T12:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: IrDA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066540#M8625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the IrDA communication pulse width.&lt;/P&gt;&lt;P&gt;The RT1064 LPUART shows Infrared decoder with Noise filtering feature:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115057i044ADE211CAE67CA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If there exists the pulse width smaller than on oversampling baud clock width?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2020 06:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066540#M8625</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2020-07-09T06:39:28Z</dc:date>
    </item>
    <item>
      <title>Re: IrDA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066541#M8626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I kind of gotten it working.&amp;nbsp; &amp;nbsp;IrDA being half duplex helps a lot if Rx or Tx one of them should be inverted so they fight less.&amp;nbsp; The baud rate still only works at 9600 when set to 32 OSR.&amp;nbsp; The pulses are all measured correctly. It gets data, but is wrong and fails my CRC check when I choose the wrong CRC.&amp;nbsp; The autobaud code in the FSL code is mildly wrong, as it trucates decimal points in the math in casting as Ints, but that didn't solve the problem either.&amp;nbsp; For now I'll just force OSR of 32 for 9600.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2020 12:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066541#M8626</guid>
      <dc:creator>sjones1</dc:creator>
      <dc:date>2020-08-04T12:30:31Z</dc:date>
    </item>
    <item>
      <title>Re: IrDA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066542#M8627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Steven,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for the feedback.&lt;/P&gt;&lt;P&gt;Could you help to provide more detailed info about this issue?&lt;/P&gt;&lt;P&gt;Such as captured communication signals, related software code, related hardware circuit.&lt;/P&gt;&lt;P&gt;Then I could ask product team to analyse this issue and try to find the root cause. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2020 14:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IrDA/m-p/1066542#M8627</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2020-08-05T14:38:19Z</dc:date>
    </item>
  </channel>
</rss>