<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1064 - any differences between 10x10 and 12x12 package sizes? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-any-differences-between-10x10-and-12x12-package-sizes/m-p/1057664#M8284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We previously designed a custom board using MIMXRT1064DVL6A, which is the 10x10 mm package.&amp;nbsp; Now that the 12x12 mm package is available, we would like to use&amp;nbsp;that instead.&amp;nbsp; Besides package size, are there any other differences between them?&amp;nbsp; We have reviewed datasheet and manual and cannot&amp;nbsp;find any differences, but want to double-check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jul 2020 02:45:30 GMT</pubDate>
    <dc:creator>jason_lo</dc:creator>
    <dc:date>2020-07-17T02:45:30Z</dc:date>
    <item>
      <title>MIMXRT1064 - any differences between 10x10 and 12x12 package sizes?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-any-differences-between-10x10-and-12x12-package-sizes/m-p/1057664#M8284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We previously designed a custom board using MIMXRT1064DVL6A, which is the 10x10 mm package.&amp;nbsp; Now that the 12x12 mm package is available, we would like to use&amp;nbsp;that instead.&amp;nbsp; Besides package size, are there any other differences between them?&amp;nbsp; We have reviewed datasheet and manual and cannot&amp;nbsp;find any differences, but want to double-check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 02:45:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-any-differences-between-10x10-and-12x12-package-sizes/m-p/1057664#M8284</guid>
      <dc:creator>jason_lo</dc:creator>
      <dc:date>2020-07-17T02:45:30Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 - any differences between 10x10 and 12x12 package sizes?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-any-differences-between-10x10-and-12x12-package-sizes/m-p/1057665#M8285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are correct, there are no differences apart from the package.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored.&lt;/P&gt;&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 18:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-any-differences-between-10x10-and-12x12-package-sizes/m-p/1057665#M8285</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-07-20T18:00:01Z</dc:date>
    </item>
  </channel>
</rss>