<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT1060 LUART1?</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1060-LUART1/m-p/794835#M818</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes "LUART1" is LPUART1. LPUART1 is also mentioned in Boot Chapter of&lt;/P&gt;&lt;P&gt;i.MXRT1050 Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Nov 2018 23:15:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-11-01T23:15:55Z</dc:date>
    <item>
      <title>RT1060 LUART1?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1060-LUART1/m-p/794834#M817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The IMXRT1060RM document has the following note at the end of Table 8-2, page 196:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE&lt;BR /&gt;1. ...&lt;BR /&gt;2. The boot ROM enables LUART1 and USB1 interrupts in&lt;BR /&gt;serial downloader mode, and it disables these interrupts&lt;BR /&gt;before jumping to user applications. However, if the boot&lt;BR /&gt;ROM execution is interrupted by the debug tool, it cannot&lt;BR /&gt;disable these interrupts; the user application needs to&lt;BR /&gt;disable these interrupts in the startup codes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please clarify "LUART1" is this really just LPUART1?&amp;nbsp; LUART1 does not appear anywhere else in the document.&amp;nbsp; This note does not appear in the RT1050 reference manual either.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 13:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1060-LUART1/m-p/794834#M817</guid>
      <dc:creator>bw1</dc:creator>
      <dc:date>2018-11-01T13:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: RT1060 LUART1?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1060-LUART1/m-p/794835#M818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes "LUART1" is LPUART1. LPUART1 is also mentioned in Boot Chapter of&lt;/P&gt;&lt;P&gt;i.MXRT1050 Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 23:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1060-LUART1/m-p/794835#M818</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-11-01T23:15:55Z</dc:date>
    </item>
  </channel>
</rss>