<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: i.MXRT1021 directly R/W AHB command without IP command</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1021-directly-R-W-AHB-command-without-IP-command/m-p/1055114#M8171</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FlexSPI peripheral does support AHB writes, but only to RAM memories that complete write commands very quickly.&amp;nbsp; For flash memories, you need to use the FlexSPI IP commands to write/erase flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;- If this post answers your question, please click the "Mark Correct"button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/P&gt;&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Aug 2020 22:55:53 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2020-08-25T22:55:53Z</dc:date>
    <item>
      <title>i.MXRT1021 directly R/W AHB command without IP command</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1021-directly-R-W-AHB-command-without-IP-command/m-p/1055113#M8170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have modified the LUT and created the corresponding read/write IP command program, and it can read/write normally.&lt;BR /&gt;Next, I want to understand how to read/write directly through AHB without using IP command&lt;BR /&gt;I ran the program in RAM, without the NOR Flash of PortA1, only the PSRAM of PortB1&lt;BR /&gt;But I don’t know how to set the address corresponding to AHB&lt;BR /&gt;I assume it starts from 0x6000 0000, but direct access to 0x6000 0000 will cause MemManage_Handler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2020 06:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1021-directly-R-W-AHB-command-without-IP-command/m-p/1055113#M8170</guid>
      <dc:creator>tim_tan</dc:creator>
      <dc:date>2020-08-21T06:13:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1021 directly R/W AHB command without IP command</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1021-directly-R-W-AHB-command-without-IP-command/m-p/1055114#M8171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FlexSPI peripheral does support AHB writes, but only to RAM memories that complete write commands very quickly.&amp;nbsp; For flash memories, you need to use the FlexSPI IP commands to write/erase flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;- If this post answers your question, please click the "Mark Correct"button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/P&gt;&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2020 22:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1021-directly-R-W-AHB-command-without-IP-command/m-p/1055114#M8171</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-08-25T22:55:53Z</dc:date>
    </item>
  </channel>
</rss>