<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: BME280 connection problem</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/BME280-connection-problem/m-p/1045836#M7778</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please provide more information about the problem that you are facing? For example, are you using our SDK? If so, which version? Do you have a logic analyzer so you can see whether the RT is sending the I2C frame correctly or not? I highly recommend you to use one of the I2C example projects that we provide within the SDK as a base for your application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Jul 2020 17:16:35 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2020-07-06T17:16:35Z</dc:date>
    <item>
      <title>BME280 connection problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/BME280-connection-problem/m-p/1045835#M7777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;BME280 chip init: ID read failed: -5&amp;nbsp;&lt;BR /&gt;Connect BME280 to iMX RT1020 through I2C4 pins D14 and D15&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2020 16:37:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/BME280-connection-problem/m-p/1045835#M7777</guid>
      <dc:creator>straton_florin_</dc:creator>
      <dc:date>2020-06-30T16:37:08Z</dc:date>
    </item>
    <item>
      <title>Re: BME280 connection problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/BME280-connection-problem/m-p/1045836#M7778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please provide more information about the problem that you are facing? For example, are you using our SDK? If so, which version? Do you have a logic analyzer so you can see whether the RT is sending the I2C frame correctly or not? I highly recommend you to use one of the I2C example projects that we provide within the SDK as a base for your application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 17:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/BME280-connection-problem/m-p/1045836#M7778</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-07-06T17:16:35Z</dc:date>
    </item>
  </channel>
</rss>