<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックUse FlexPWM output as QTimer clock</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-FlexPWM-output-as-QTimer-clock/m-p/1040686#M7563</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a FlexPWM to generate the step signal for a stepper motor driver chip. I want to keep an exact count of the number of steps I command to the chip. My plan is to route the FlexPWM output to a QTimer, but I'm a bit confused on how to go about doing this. I'll need to setup the pinmux appropriately of course.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming I can jumper a wire from the PWM pin to an input pin, how do I configure the QTimer block? Can I skip the jumper wire and simply use the Xbar for this? I'm fairly new to the RT so this has me stumped for now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jun 2020 00:20:33 GMT</pubDate>
    <dc:creator>kendalla59</dc:creator>
    <dc:date>2020-06-02T00:20:33Z</dc:date>
    <item>
      <title>Use FlexPWM output as QTimer clock</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-FlexPWM-output-as-QTimer-clock/m-p/1040686#M7563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a FlexPWM to generate the step signal for a stepper motor driver chip. I want to keep an exact count of the number of steps I command to the chip. My plan is to route the FlexPWM output to a QTimer, but I'm a bit confused on how to go about doing this. I'll need to setup the pinmux appropriately of course.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming I can jumper a wire from the PWM pin to an input pin, how do I configure the QTimer block? Can I skip the jumper wire and simply use the Xbar for this? I'm fairly new to the RT so this has me stumped for now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 00:20:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-FlexPWM-output-as-QTimer-clock/m-p/1040686#M7563</guid>
      <dc:creator>kendalla59</dc:creator>
      <dc:date>2020-06-02T00:20:33Z</dc:date>
    </item>
    <item>
      <title>Re: Use FlexPWM output as QTimer clock</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-FlexPWM-output-as-QTimer-clock/m-p/1040687#M7564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kendall,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I recommend you to check our qtmr_inputcapture_outputpwm SDK example. You can download the SDK in this link.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This project is a demonstration of the SDK QTMR driver's input capture and output pwm feature.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored.&lt;/P&gt;&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 22:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-FlexPWM-output-as-QTimer-clock/m-p/1040687#M7564</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-06-04T22:01:38Z</dc:date>
    </item>
  </channel>
</rss>