<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Are there clear indicators that ERR050101 is occuring? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Are-there-clear-indicators-that-ERR050101-is-occuring/m-p/1039296#M7516</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running into an issue on the RT1051. The device has isochronous USB IN and OUT endpoints. When connected to certain hosts (both directly and through a hub) the USB audio device enumerates properly and the host sends isochronous data to the device, however the OTG1_IRQHandler is not invoked by the isochronous packets. I am wondering if the issue I am seeing is related to the 'ERR050101 USB: Endpoint conflict issue in device mode' defect as described in Chip Errata for the i.MX RT1050, Rev. 2.2 (see attached).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any clear indicators that I can observe using my IDE and debugger to determine if&amp;nbsp;&lt;SPAN&gt;ERR050101&amp;nbsp;is occurring?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Michael&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jun 2020 17:21:32 GMT</pubDate>
    <dc:creator>michael_adams</dc:creator>
    <dc:date>2020-06-12T17:21:32Z</dc:date>
    <item>
      <title>Are there clear indicators that ERR050101 is occuring?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Are-there-clear-indicators-that-ERR050101-is-occuring/m-p/1039296#M7516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running into an issue on the RT1051. The device has isochronous USB IN and OUT endpoints. When connected to certain hosts (both directly and through a hub) the USB audio device enumerates properly and the host sends isochronous data to the device, however the OTG1_IRQHandler is not invoked by the isochronous packets. I am wondering if the issue I am seeing is related to the 'ERR050101 USB: Endpoint conflict issue in device mode' defect as described in Chip Errata for the i.MX RT1050, Rev. 2.2 (see attached).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any clear indicators that I can observe using my IDE and debugger to determine if&amp;nbsp;&lt;SPAN&gt;ERR050101&amp;nbsp;is occurring?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Michael&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2020 17:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Are-there-clear-indicators-that-ERR050101-is-occuring/m-p/1039296#M7516</guid>
      <dc:creator>michael_adams</dc:creator>
      <dc:date>2020-06-12T17:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: Are there clear indicators that ERR050101 is occuring?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Are-there-clear-indicators-that-ERR050101-is-occuring/m-p/1039297#M7517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Michael,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, there is no flag or specific register that could tell us that the errata is occurring. However, if you are in the same scenario as described in ERR050101&amp;nbsp;when ISO IN endpoint is used and the corresponding interrupt is not occurring then we can infer you are facing same issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 15:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Are-there-clear-indicators-that-ERR050101-is-occuring/m-p/1039297#M7517</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-06-16T15:45:16Z</dc:date>
    </item>
  </channel>
</rss>