<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT1020, SD and QSPI with LQFP100</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790601#M727</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have designed my own custom board&amp;nbsp;with the RT1020 LQFP100. I have read the Reference Manual and the Data Sheet, but I am still not sure if I can connect the QSPI and the SD, both to GPIO_SD_B1. I see that there is a second option for QSPI in GPIO_AD_B1, but I need those pins for JTAG or SWD, to do Debug and to program with MCUXpresso, so I decided to connect the QSPI to GPIO_SD_B1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached images of my custom board PCB, and where I have connected the SD and the QSPI in GPIO_SD_B1. Can someone confirm that it is correct? I will receive the PCB in a week, then I will assemble and test everything.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have read in the Reference Manual and in the Data Sheet, about the boot modes and IOMUX, but I do not know if when I choose to start from QSPI, the microcontroller can automatically choose any of the two FlexSPI options for QSPI, GPIO_SD_B1 or GPIO_AD_B1 , and if there can be any conflict if SD and QSPI are both in GPIO_SD_B1.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sincerely&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_030.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62753iD279748C94A8AC13/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_030.jpg" alt="ScreenHunter_030.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="R3qtuAS.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62799iD332594C4D8179E2/image-size/large?v=v2&amp;amp;px=999" role="button" title="R3qtuAS.jpg" alt="R3qtuAS.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_031.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62815iB4D043981C4F45E0/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_031.jpg" alt="ScreenHunter_031.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Aug 2018 23:35:17 GMT</pubDate>
    <dc:creator>luishs</dc:creator>
    <dc:date>2018-08-14T23:35:17Z</dc:date>
    <item>
      <title>RT1020, SD and QSPI with LQFP100</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790598#M724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I am designing a product with the RT1020 LQFP100 microcontroller, I am based on the schematics of the MIMXRT1020-EVK evaluation board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that the MIMXRT1020-EVK board installs an LQFP144, and I'm going to use an LQFP100 (the only one currently available, otherwise I would have used an LQFP144 that interests me more). This affects the design of the boot with SD card and QSPI. I see in the diagrams of the evaluation board, that the SD card is connected to the ports GPIO_SD_B0_ and the QSPI to the ports GPIO_SD_B1_.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the LQFP100, the GPIO_SD_B0_ port does not exist, and that is my problem, where to connect the SD card and the QSPI in an LQFP100.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that the SD card must be connected to the GPIO_SD_B1_ ports with the same numbering that the evaluation board connects to the GPIO_SD_B0_ but I am not sure. On the other hand, the QSPI could also be connected to the GPIO_SD_B1_ ports, but in that case the GPIO_SD_B1_06 port is shared between the SD and the QSPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All this, unless the QSPI must be really connected to the "FlexSPI2nd Option" ports, GPIO_AD_B1_.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone confirm where the SD card and QSPI are connected to an RT1020 LQFP100?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_247.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66613iFA7FC3C1BB9F6F59/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_247.jpg" alt="ScreenHunter_247.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SD2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66614i225C7BBF01C62EB6/image-size/large?v=v2&amp;amp;px=999" role="button" title="SD2.jpg" alt="SD2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_250.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66615iBE1569C522D7FBA1/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_250.jpg" alt="ScreenHunter_250.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_251.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66616i4FB877DF8E2FAD1D/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_251.jpg" alt="ScreenHunter_251.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 18:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790598#M724</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-07-26T18:59:41Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020, SD and QSPI with LQFP100</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790599#M725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you refer to i.MXRT1020 Datasheet, Table 1 “The comparison between 100 LQFP and 144 LQFP package”, mentions that there is only one uSDHC module on 100-pin package:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/IMXRT1020IEC.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/IMXRT1020IEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Additionally, on i.MXRT1020 Reference Manual Table 8-33 “IOMUX configuration for SD/MMC”, the pin distribution is summarized for both SD controllers of the processor:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMXRT1020RM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/IMXRT1020RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You could also take a look to tables 70, 71, 72, 73 and 74 of i.MXRT1020 Datasheet for specific pin muxing options for SD and FlexSPI modules.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 20:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790599#M725</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-07-30T20:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020, SD and QSPI with LQFP100</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790600#M726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, thanks Carlos.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Aug 2018 08:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790600#M726</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-08-08T08:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020, SD and QSPI with LQFP100</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790601#M727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have designed my own custom board&amp;nbsp;with the RT1020 LQFP100. I have read the Reference Manual and the Data Sheet, but I am still not sure if I can connect the QSPI and the SD, both to GPIO_SD_B1. I see that there is a second option for QSPI in GPIO_AD_B1, but I need those pins for JTAG or SWD, to do Debug and to program with MCUXpresso, so I decided to connect the QSPI to GPIO_SD_B1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached images of my custom board PCB, and where I have connected the SD and the QSPI in GPIO_SD_B1. Can someone confirm that it is correct? I will receive the PCB in a week, then I will assemble and test everything.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have read in the Reference Manual and in the Data Sheet, about the boot modes and IOMUX, but I do not know if when I choose to start from QSPI, the microcontroller can automatically choose any of the two FlexSPI options for QSPI, GPIO_SD_B1 or GPIO_AD_B1 , and if there can be any conflict if SD and QSPI are both in GPIO_SD_B1.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sincerely&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_030.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62753iD279748C94A8AC13/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_030.jpg" alt="ScreenHunter_030.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="R3qtuAS.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62799iD332594C4D8179E2/image-size/large?v=v2&amp;amp;px=999" role="button" title="R3qtuAS.jpg" alt="R3qtuAS.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_031.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62815iB4D043981C4F45E0/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_031.jpg" alt="ScreenHunter_031.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 23:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790601#M727</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-08-14T23:35:17Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020, SD and QSPI with LQFP100</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790602#M728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Luis,&lt;/P&gt;&lt;P&gt;I'm solving the same problem now. I need to connect quad SPI NOR and SD card to this chip. I supposed the same solution as you, when I repeatedly reading so thick datasheet.&lt;/P&gt;&lt;P&gt;What is your result for this issue? Disclose, please.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Palo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 13:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-SD-and-QSPI-with-LQFP100/m-p/790602#M728</guid>
      <dc:creator>pavelspanik</dc:creator>
      <dc:date>2019-01-11T13:53:27Z</dc:date>
    </item>
  </channel>
</rss>