<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX RT1020, FlexSPI and 1.8V Flash? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1020-FlexSPI-and-1-8V-Flash/m-p/1031463#M7203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jing,&lt;/P&gt;&lt;P&gt;thanks for the answer, even though it wasn't the answer I would like to get.&lt;/P&gt;&lt;P&gt;Most of the Flashes with Octal SPI interface and RWW capability are 1.8V flashes. So for applications where we use XIP and some kind of data flash we will need 2 flashes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Gerhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Feb 2020 07:24:13 GMT</pubDate>
    <dc:creator>gerhardf</dc:creator>
    <dc:date>2020-02-17T07:24:13Z</dc:date>
    <item>
      <title>i.MX RT1020, FlexSPI and 1.8V Flash?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1020-FlexSPI-and-1-8V-Flash/m-p/1031461#M7201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;would it be possible to connect a 1.8V Octal SPI Flash (like the Adesto ATX064P)&amp;nbsp;via FlexSPI to a i.MX RT1020?&lt;/P&gt;&lt;P&gt;The schematic of the&amp;nbsp;i.MX RT1020 EVK shows this possibility.&amp;nbsp;NVCC_SD is switchable between 1.8V and 3.3V (see page 4).&lt;/P&gt;&lt;P&gt;But according to the reference manual, Table 83, Ports&amp;nbsp;GPIO_SD_B1_xx are supplied by&amp;nbsp;NVCC_GPIO which is 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Gerhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 09:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1020-FlexSPI-and-1-8V-Flash/m-p/1031461#M7201</guid>
      <dc:creator>gerhardf</dc:creator>
      <dc:date>2020-02-14T09:26:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT1020, FlexSPI and 1.8V Flash?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1020-FlexSPI-and-1-8V-Flash/m-p/1031462#M7202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gerhard,&lt;/P&gt;&lt;P&gt;No, RT1020 can't support 1.8v Octal QSPI. You can see in the table 83 that RT1021 even haven't so much NVCC_SD0 field pads.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 03:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1020-FlexSPI-and-1-8V-Flash/m-p/1031462#M7202</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-02-17T03:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT1020, FlexSPI and 1.8V Flash?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1020-FlexSPI-and-1-8V-Flash/m-p/1031463#M7203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jing,&lt;/P&gt;&lt;P&gt;thanks for the answer, even though it wasn't the answer I would like to get.&lt;/P&gt;&lt;P&gt;Most of the Flashes with Octal SPI interface and RWW capability are 1.8V flashes. So for applications where we use XIP and some kind of data flash we will need 2 flashes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Gerhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 07:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1020-FlexSPI-and-1-8V-Flash/m-p/1031463#M7203</guid>
      <dc:creator>gerhardf</dc:creator>
      <dc:date>2020-02-17T07:24:13Z</dc:date>
    </item>
  </channel>
</rss>