<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mfgtool maks FreeRTOS wrong in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/mfgtool-maks-FreeRTOS-wrong/m-p/715385#M7</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is an i.MXRT1050 platform, my project&amp;nbsp;including FreeRTOS run as XIP in a QSPI flash,&lt;/P&gt;&lt;P&gt;if programming by IAR-Jlink, then reset the board to run it, everything is fine (I have created IVT and flash configuration block manually in source code).&lt;/P&gt;&lt;P&gt;But if programming by mfgtool, system runs, but crashed at last sentence of vPortStartFirstTask();&lt;/P&gt;&lt;P&gt;if remove FReeRTOS, and copy the task content to main(), everything is fine too after mfgtool programming.&lt;/P&gt;&lt;P&gt;By checking the content of flash, flash configuration block (0x60000000-0x60000FFF) and IVT (0x60000100-0x60001FFF) are little different, but application (0x60002000-0x6000xxxx) is the same. Normally, mfgtool only add some headers of application, but the action is different between both programming ways? It's so interesting, anyone knows the reason?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Apr 2018 09:22:17 GMT</pubDate>
    <dc:creator>ffloree</dc:creator>
    <dc:date>2018-04-09T09:22:17Z</dc:date>
    <item>
      <title>mfgtool maks FreeRTOS wrong</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/mfgtool-maks-FreeRTOS-wrong/m-p/715385#M7</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is an i.MXRT1050 platform, my project&amp;nbsp;including FreeRTOS run as XIP in a QSPI flash,&lt;/P&gt;&lt;P&gt;if programming by IAR-Jlink, then reset the board to run it, everything is fine (I have created IVT and flash configuration block manually in source code).&lt;/P&gt;&lt;P&gt;But if programming by mfgtool, system runs, but crashed at last sentence of vPortStartFirstTask();&lt;/P&gt;&lt;P&gt;if remove FReeRTOS, and copy the task content to main(), everything is fine too after mfgtool programming.&lt;/P&gt;&lt;P&gt;By checking the content of flash, flash configuration block (0x60000000-0x60000FFF) and IVT (0x60000100-0x60001FFF) are little different, but application (0x60002000-0x6000xxxx) is the same. Normally, mfgtool only add some headers of application, but the action is different between both programming ways? It's so interesting, anyone knows the reason?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 09:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/mfgtool-maks-FreeRTOS-wrong/m-p/715385#M7</guid>
      <dc:creator>ffloree</dc:creator>
      <dc:date>2018-04-09T09:22:17Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool maks FreeRTOS wrong</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/mfgtool-maks-FreeRTOS-wrong/m-p/715386#M8</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason may be that mfg tool uses some standard typical settings described in&lt;BR /&gt;sect.8.2.2.1 Typical use cases for FlexSPI NOR Configuration Block&lt;BR /&gt;MCUX Flashloader Reference Manual.pdf included in FlashLoader package.&lt;BR /&gt;Usage can be checked in AN12108&amp;nbsp; How to Enable Boot from QSPI Flash&lt;BR /&gt;Figure 15. Modify the parameter from 0xc0233007 to 0xc0000005.&lt;BR /&gt;DCD header can be tweaked with example in AN12107 How to Enable Boot from &lt;BR /&gt;HyperFlash and SD Card: dcd in file *.bd:&lt;BR /&gt;Figure 38. Add DCD path,&amp;nbsp; options { DCDFilePath,&lt;BR /&gt;described in sect.4.1.3.1. Options block i.MX MCU Manufacturing User's Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 23:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/mfgtool-maks-FreeRTOS-wrong/m-p/715386#M8</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-09T23:01:25Z</dc:date>
    </item>
  </channel>
</rss>