<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX28 SPI Problem in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX28-SPI-Problem/m-p/788277#M684</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been working with TQMA28 ( IMX28 Processor ) board. I need to implement wilc1000 wifi module to the stater kit. But I have an issue about the SPI. The atwilc1000 wifi module is full duplex spi slave and IMX28 is working only half duplex spi master mode.&amp;nbsp;&lt;SPAN&gt;I have read about this issue in that forum,but there are no solution about how to make the IMX28 SPI work as full duplex.&amp;nbsp;&lt;/SPAN&gt;I implemented wifi module device driver to the linux and then I tried it make it work, but wifi module have to speak with host with full duplex mode. So I need solution or recomendation about at kernel level programming or modification.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;would be very greatful&amp;nbsp;any recomendations and ideas. Besides that, If you have any linux kernel gpio-bitbanging example about the spi it would be helpful too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mustafa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2018 15:33:21 GMT</pubDate>
    <dc:creator>mustafa_bakirci</dc:creator>
    <dc:date>2018-11-21T15:33:21Z</dc:date>
    <item>
      <title>IMX28 SPI Problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX28-SPI-Problem/m-p/788277#M684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been working with TQMA28 ( IMX28 Processor ) board. I need to implement wilc1000 wifi module to the stater kit. But I have an issue about the SPI. The atwilc1000 wifi module is full duplex spi slave and IMX28 is working only half duplex spi master mode.&amp;nbsp;&lt;SPAN&gt;I have read about this issue in that forum,but there are no solution about how to make the IMX28 SPI work as full duplex.&amp;nbsp;&lt;/SPAN&gt;I implemented wifi module device driver to the linux and then I tried it make it work, but wifi module have to speak with host with full duplex mode. So I need solution or recomendation about at kernel level programming or modification.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;would be very greatful&amp;nbsp;any recomendations and ideas. Besides that, If you have any linux kernel gpio-bitbanging example about the spi it would be helpful too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mustafa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 15:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX28-SPI-Problem/m-p/788277#M684</guid>
      <dc:creator>mustafa_bakirci</dc:creator>
      <dc:date>2018-11-21T15:33:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 SPI Problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX28-SPI-Problem/m-p/788278#M685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mustafa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX28 spi limitations and workarounds are described on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317317"&gt;Can the imx28 spi work in duplex mode&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for usage spi bitbanging oen can look on common linux resources like:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://stackoverflow.com/questions/30789296/bit-bang-with-spi-fwirte-write-performance" title="https://stackoverflow.com/questions/30789296/bit-bang-with-spi-fwirte-write-performance"&gt;linux - Bit Bang with SPI (fwirte, write performance) - Stack Overflow&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2018 07:58:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX28-SPI-Problem/m-p/788278#M685</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-11-26T07:58:24Z</dc:date>
    </item>
  </channel>
</rss>