<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Not having any success with flashloader for '1020...</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-having-any-success-with-flashloader-for-1020/m-p/1018359#M6751</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running into a few problems getting started with my MIMXRT1020EVK, so I decided&amp;nbsp;to just follow the steps in the "&lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf"&gt;Flashloader Use Case&lt;/A&gt;" document that comes with the flashloader package for the MIMXRT1020EVK (Flashloader_RT1020_1.0_GA)...&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Referring to that document and the directory that comes with the package, I ran the following commands:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;sdphost -u 0x1fc9,0x0130 -- error-status&lt;/LI&gt;&lt;LI&gt;sdphost -u 0x1fc9,0x0130 -- write-file 0x20000000 "Tools/mfgtools-rel/Profiles/MXRT102X/OS&amp;nbsp; Firmware/ivt_flashloader.bin"&lt;/LI&gt;&lt;LI&gt;sdphost -u 0x1fc9,0x0130 -- jump-address 0x20000400&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each of these commands worked, but the sanity test (as per the document) failed...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;blhost -u -- get-property 1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;The USB port is apparently supposed to re-enumerate to a different VID/PID, but it doesn't.&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Feb 2020 20:34:41 GMT</pubDate>
    <dc:creator>EdSutter</dc:creator>
    <dc:date>2020-02-26T20:34:41Z</dc:date>
    <item>
      <title>Not having any success with flashloader for '1020...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-having-any-success-with-flashloader-for-1020/m-p/1018359#M6751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running into a few problems getting started with my MIMXRT1020EVK, so I decided&amp;nbsp;to just follow the steps in the "&lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf"&gt;Flashloader Use Case&lt;/A&gt;" document that comes with the flashloader package for the MIMXRT1020EVK (Flashloader_RT1020_1.0_GA)...&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Referring to that document and the directory that comes with the package, I ran the following commands:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;sdphost -u 0x1fc9,0x0130 -- error-status&lt;/LI&gt;&lt;LI&gt;sdphost -u 0x1fc9,0x0130 -- write-file 0x20000000 "Tools/mfgtools-rel/Profiles/MXRT102X/OS&amp;nbsp; Firmware/ivt_flashloader.bin"&lt;/LI&gt;&lt;LI&gt;sdphost -u 0x1fc9,0x0130 -- jump-address 0x20000400&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each of these commands worked, but the sanity test (as per the document) failed...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;blhost -u -- get-property 1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;The USB port is apparently supposed to re-enumerate to a different VID/PID, but it doesn't.&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 20:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-having-any-success-with-flashloader-for-1020/m-p/1018359#M6751</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2020-02-26T20:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: Not having any success with flashloader for '1020...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-having-any-success-with-flashloader-for-1020/m-p/1018360#M6752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Turns out that the addresses passed to sdphost are different.&amp;nbsp; For details on that refer to &lt;A _jive_internal="true" href="https://community.nxp.com/message/1275013"&gt;this &lt;/A&gt;post.&lt;/P&gt;&lt;P&gt;In the nutshell...&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;sdphost -u 0x1fc9,0x0130 -- write-file 0x20208000...&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;sdphost -u 0x1fc9,0x0130 -- jump-address 0x20208400&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;work much better.&amp;nbsp; Thanks to the originator of that post.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 19:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-having-any-success-with-flashloader-for-1020/m-p/1018360#M6752</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2020-02-27T19:36:19Z</dc:date>
    </item>
  </channel>
</rss>