<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SD Power Enable in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017626#M6739</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update:&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found this issue because I was having issues with the sd at boot(some cards would work and others would not). However, I recently updated to the newest SDK_2.7.0_EVK-MIMXRT1064 and it seems to fix the original problem I was having, but I am still seeing some leakage back on VDD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jan 2020 21:11:11 GMT</pubDate>
    <dc:creator>vonp</dc:creator>
    <dc:date>2020-01-21T21:11:11Z</dc:date>
    <item>
      <title>SD Power Enable</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017623#M6736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom board based off of the RT1064-EVK. I am having issues resetting the SD card VDD using M12 GPIO_AD_B1_03 and a simple p-channel mosfet in a high side switch configuration. I have tested this circuit with a restive load at around 300mA with the SD card removed and it works fine.&amp;nbsp;However, when the SD card is inserted and I pull M12 low I measure about 2.3V DC. It seems that there is some leakage current from the SD card IO pins back on VDD. I have compared this to the EVK which does not show this error(unless the SD data lines are driven high then I do, but not in the SD driver demo example). Is there anything I am missing? Why can I not drive VDD low?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="RT_SD.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91305i6E0DFD9D8D1F09EE/image-size/large?v=v2&amp;amp;px=999" role="button" title="RT_SD.JPG" alt="RT_SD.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 21:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017623#M6736</guid>
      <dc:creator>vonp</dc:creator>
      <dc:date>2020-01-15T21:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: SD Power Enable</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017624#M6737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Heath,&lt;/P&gt;&lt;P&gt;You schematic looks fine. I also test on my EVB. When GPIO_AD_B1_03 output 0, SD card VDD is also 0. Did you measure Q1 gate voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 05:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017624#M6737</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-01-17T05:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: SD Power Enable</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017625#M6738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I checked the gate voltage on Q1 and looks correct. Like I said above if the SD card is removed Q1 operates as it should, I have also only connected VDD and VSS on the SD card and it operates correctly, but once I connect the data pins it reads VDD at 2.4VDC when off and 3.3VDC when on.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 21:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017625#M6738</guid>
      <dc:creator>vonp</dc:creator>
      <dc:date>2020-01-21T21:06:39Z</dc:date>
    </item>
    <item>
      <title>Re: SD Power Enable</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017626#M6739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update:&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found this issue because I was having issues with the sd at boot(some cards would work and others would not). However, I recently updated to the newest SDK_2.7.0_EVK-MIMXRT1064 and it seems to fix the original problem I was having, but I am still seeing some leakage back on VDD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 21:11:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017626#M6739</guid>
      <dc:creator>vonp</dc:creator>
      <dc:date>2020-01-21T21:11:11Z</dc:date>
    </item>
    <item>
      <title>Re: SD Power Enable</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017627#M6740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, it seems the voltage comes from SD card data pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2020 06:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Power-Enable/m-p/1017627#M6740</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-01-22T06:47:04Z</dc:date>
    </item>
  </channel>
</rss>