<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1052 1V2 rail in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787277#M668</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I can see that they are both high (3.3 volts). In the screenshot below the blue trace is the VDD_HIGH, VDDA_ADC_3P3, and DCDC rails (they are all joined together, the SNVS comes up 250 ms before). The yellow trace is the PSWITCH and the purple trace is the VDD_SOC_IN (1V2 rail). PMIC_ON_REQ is connected to the enable line of the DCDC reg so comes up just before the DCDC rail.&lt;span class="lia-inline-image-display-wrapper" image-alt="tek00000.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63197i50402883DA08EE01/image-size/large?v=v2&amp;amp;px=999" role="button" title="tek00000.png" alt="tek00000.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Aug 2018 13:07:41 GMT</pubDate>
    <dc:creator>martinsmith</dc:creator>
    <dc:date>2018-08-16T13:07:41Z</dc:date>
    <item>
      <title>RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787266#M657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am bring up a custom PCB and the SNVS, DCDC and 3V3 rails all come up OK in the right order. As a result I was expecting the 1V2 rail to come up to power the M7 core, but it doesn't. I have the inductor and caps connected right but nothing. Is there anything I have to do to enable it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 15:59:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787266#M657</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-14T15:59:24Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787267#M658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check design, also paying attention to clocks, using&lt;/P&gt;&lt;P&gt;sect.3. Power supply, sect.4. Clocks&lt;/P&gt;&lt;P&gt;Hardware Development Guide for the MIMXRT1050 Processor &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/MIMXRT1050HDUG.pdf"&gt;https://www.nxp.com/docs/en/user-guide/MIMXRT1050HDUG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 05:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787267#M658</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-15T05:42:00Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787268#M659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks for your help.&lt;/P&gt;&lt;P&gt;I've been looking at it this morning. The SNVS rail (3V3) comes up first, along with the DCDC rail (3V). I can see the&amp;nbsp;DCDC start to come up (PSWITCH is high around 1ms after DCDC). The&amp;nbsp;1V2 rail (VDD_SOC_IN, aka the output from the internal&amp;nbsp;DCDC) rises to around 1V then gets very noisy. At this point the DCDC rail dips and the 1V2 rail collapses.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have had a good look through the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hardware Development Guide for the MIMXRT1050 Processor&lt;SPAN&gt;&amp;nbsp;and can't see what i'm doing wrong.&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DCDC rail just goes to balls L1, L2 and K4, and the 1V2 rail coming out of the inductor / Cap filter just goes to the VDD_SOC_IN balls and the DCDC_SENSE ball (J5). I have all the required caps fitted around the RT1052.&lt;/P&gt;&lt;P&gt;I am using rev B silicon if that makes any difference?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 11:54:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787268#M659</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-15T11:54:20Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787269#M660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;so do you have working clocks in XTALI/XTALO, RTC_XTALI/RTC_XTALO,&lt;/P&gt;&lt;P&gt;may be useful to look at Figure 45-1. Power system overview i.MX RT1050 Processor Reference Manual&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;sect.4.2.2 Integrated LDO voltage regulator parameters, sect.4.2.4 On-chip oscillators&lt;/P&gt;&lt;P&gt;i.MXRT1050 Datasheet &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fdata-sheet%2FIMXRT1050CEC.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/IMXRT1050CEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 12:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787269#M660</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-15T12:00:48Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787270#M661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No the clocks are not working - but I think this is because they are powered from VDD_SOC_IN? I don't have an RTC clock fitted anyway.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 13:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787270#M661</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-15T13:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787271#M662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;according to sect.4.2.4.2 OSC32K - it is powered from VDD_SNVS_IN.&lt;/P&gt;&lt;P&gt;from sect.4.2.4.1 OSC24M - it is powered from NVCC_PLL.&lt;/P&gt;&lt;P&gt;from Figure 45-1 - NVCC_PLL produced from NVDD_HIGH_IN through LDO_1P1.&lt;/P&gt;&lt;P&gt;So seems they all should work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 13:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787271#M662</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-15T13:51:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787272#M663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OSC32K appears to be the RTC - which I am not using (N9 tied to GND and P9 floating)&lt;/P&gt;&lt;P&gt;NVCC_PLL is connected to ball P10 (from Table 81) - which I can check and confirm has 1.1V on it. But VDD_HIGH_IN is powered up after DCDC so shouldn't be interfering with VDD_SOC_IN should it?&lt;/P&gt;&lt;P&gt;I will try to get the 24MHz clock working in the meantime&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 14:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787272#M663</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-15T14:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787273#M664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: Using the Eval PCB (MIMXRT1050-EVK) I have been testing the clock and VDD_SOC_IN rail.&lt;/P&gt;&lt;P&gt;1. I can see that the VDD_SOC_IN comes up around 270ms before the 24 MHz xtal starts oscillating&lt;/P&gt;&lt;P&gt;2. If I remove J36 to stop the VDD_SOC_IN rail from coming up the 24 MHZ xtal never starts ups. I can see repeated attempts about every 270ms where it tries to start but fails.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my PCB the XTAL never even tries to start.&lt;/P&gt;&lt;P&gt;So the DCDC seems to be able to interfere with the XTAL operation, even though it doesn't power it directly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 07:43:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787273#M664</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-16T07:43:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787274#M665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NVCC_PLL does not depend on VDD_SOC_IN rail, it is produced from VDD_HIGH_IN.&lt;/P&gt;&lt;P&gt;Do you have VDD_HIGH_IN, VDD_HIGH_CAP, NVCC_PLL powered ?&lt;/P&gt;&lt;P&gt;For dcdc one also can look at AN12146 Table 2 "Power", notes for DCDC_PSWITCH&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/nxp/application-notes/AN12146.pdf" title="https://www.nxp.com/docs/en/nxp/application-notes/AN12146.pdf"&gt;https://www.nxp.com/docs/en/nxp/application-notes/AN12146.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 10:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787274#M665</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-16T10:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787275#M666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_HIGH_IN, VDD_HIGH_CAP and NVCC_PLL are all powered. I have looked at the app note and have made any adjustments but still no 24 MHz xtal output and no VDD_SOC_IN&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 10:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787275#M666</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-16T10:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787276#M667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can check PMIC_ON_REQ, as described in sect.20.5.1 Turn on DCDC i.MXRT1050 RM:&lt;BR /&gt;To turn on the DCDC, PSWITCH and PMIC_ON_REQ must be both high&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 11:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787276#M667</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-16T11:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787277#M668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I can see that they are both high (3.3 volts). In the screenshot below the blue trace is the VDD_HIGH, VDDA_ADC_3P3, and DCDC rails (they are all joined together, the SNVS comes up 250 ms before). The yellow trace is the PSWITCH and the purple trace is the VDD_SOC_IN (1V2 rail). PMIC_ON_REQ is connected to the enable line of the DCDC reg so comes up just before the DCDC rail.&lt;span class="lia-inline-image-display-wrapper" image-alt="tek00000.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63197i50402883DA08EE01/image-size/large?v=v2&amp;amp;px=999" role="button" title="tek00000.png" alt="tek00000.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 13:07:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787277#M668</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-16T13:07:41Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787278#M669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;actually in the screenshot above the blue trace is sagging below 2V which violates power-up sequence and&lt;BR /&gt;voltage levels for VDD_HIGH, DCDC rails (min. about 2.8-3.0V depending on chip revision).&lt;BR /&gt;They should be smooth and its levels comply with Table 9. Operating ranges i.MX RT1050 Datasheet &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fdata-sheet%2FIMXRT1050CEC.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/IMXRT1050CEC.pdf&lt;/A&gt;&lt;BR /&gt;Reason for voltages sagging may be layout errors (short circuits, broken traces), too big capacitors&lt;BR /&gt;(check sect.7.2. Placement of bulk and decoupling capacitors Hardware Development Guide &lt;BR /&gt;for the MIMXRT1050 Processor), insufficient power supply current which feeds processor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 23:42:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787278#M669</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-16T23:42:29Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787279#M670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;UPDATE: I populated another PCB and all the rails come up OK now. I guess I can put this one down to manufacturing issues?&lt;/P&gt;&lt;P&gt;Thanks for the advise&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 11:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787279#M670</guid>
      <dc:creator>martinsmith</dc:creator>
      <dc:date>2018-08-17T11:13:06Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 1V2 rail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787280#M671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63084i736A2094243C02B2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.jpg" alt="pastedImage_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 11:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-1V2-rail/m-p/787280#M671</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-17T11:38:23Z</dc:date>
    </item>
  </channel>
</rss>