<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SD Card support issues in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011651#M6503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In SD card standard, there is default two regulator. Vmmc is operation voltage. It is from 2.7~3.6V. It connect to card vdd. Vqmmc is signal voltage, could be 1.8v/3.3v.&lt;/P&gt;&lt;P&gt;Maybe you should try another 4GB Scandisk card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Feb 2020 16:24:17 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2020-02-14T16:24:17Z</dc:date>
    <item>
      <title>SD Card support issues</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011648#M6500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gents,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I'm trying to use the following common SD Card with the Eval kit and SDcard SDK example code. However, it is working inconsistently. Failing ~50% of the time.&lt;BR /&gt;&lt;BR /&gt;Could someone explain what the issue and/or limitation is here with these cards?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99921iD87667E5B185D8BE/image-size/large?v=v2&amp;amp;px=999" title="83541382_640899493322538_7823467535948316672_n.jpg" alt="83541382_640899493322538_7823467535948316672_n.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;A href="https://www.amazon.com/gp/product/B003HIWHN0/ref=ppx_yo_dt_b_search_asin_title?ie=UTF8&amp;amp;psc=1"&gt;https://www.amazon.com/gp/product/B003HIWHN0/ref=ppx_yo_dt_b_search_asin_title?ie=UTF8&amp;amp;psc=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(WORKING)------------&lt;/P&gt;&lt;P&gt;FATFS example to demonstrate how to use FATFS with SD card.&lt;/P&gt;&lt;P&gt;Please insert a card into board.&lt;/P&gt;&lt;P&gt;Card inserted.&lt;/P&gt;&lt;P&gt;Make file system......The time may be long if the card capacity is big.&lt;/P&gt;&lt;P&gt;Create directory......&lt;/P&gt;&lt;P&gt;Create a file in that directory......&lt;/P&gt;&lt;P&gt;Create a directory in that directory......&lt;/P&gt;&lt;P&gt;List the file in that directory......&lt;BR /&gt;General file : F_1.DAT.&lt;BR /&gt;Directory file : DIR_2.&lt;/P&gt;&lt;P&gt;Write/read file until encounters error......&lt;/P&gt;&lt;P&gt;Write to above created file.&lt;BR /&gt;Read from above created file.&lt;BR /&gt;Compare the read/write content......&lt;BR /&gt;The read/write content is consistent.&lt;/P&gt;&lt;P&gt;Input 'q' to quit read/write.&lt;BR /&gt;Input other char to read/write file again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(FAILURE)----------------------&lt;BR /&gt;FATFS example to demonstrate how to use FATFS with SD card.&lt;/P&gt;&lt;P&gt;Please insert a card into board.&lt;/P&gt;&lt;P&gt;Card inserted.&lt;/P&gt;&lt;P&gt;Make file system......The time may be long if the card capacity is big.&lt;/P&gt;&lt;P&gt;Create directory......&lt;BR /&gt;Make directory failed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2020 20:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011648#M6500</guid>
      <dc:creator>mspenard603</dc:creator>
      <dc:date>2020-01-28T20:24:03Z</dc:date>
    </item>
    <item>
      <title>Re: SD Card support issues</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011649#M6501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;Is there any progress? I tested on my board again. It works fine. I guess this maybe the sd card problem. Can you change a new card and try again?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Feb 2020 10:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011649#M6501</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-02-02T10:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: SD Card support issues</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011650#M6502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well the root cause was (which I forgot about) our PCB provides only 3.3v to the SD card. So the resolution was to specify&amp;nbsp;BOARD_SD_SUPPORT_180V 0 (false) as a #symbol.&lt;BR /&gt;&lt;BR /&gt;What I don't understand is why the voltage auto-detect function in the SDK works on some cards and not others. As this 32GB SanDisk card above fails to work with the SDK voltage auto-detect. BUT the "same" card in a 4GB variant does work. Any thoughts on this would be helpful.&lt;BR /&gt;&lt;BR /&gt;Making matters more confusing is this is not always reported as a kStatus_SDMMC_SwitchVoltageFail&amp;nbsp; but sometimes a _SenddScrFailed. Which is what led to my above oversight and this post.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2020 14:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011650#M6502</guid>
      <dc:creator>mspenard603</dc:creator>
      <dc:date>2020-02-04T14:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: SD Card support issues</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011651#M6503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In SD card standard, there is default two regulator. Vmmc is operation voltage. It is from 2.7~3.6V. It connect to card vdd. Vqmmc is signal voltage, could be 1.8v/3.3v.&lt;/P&gt;&lt;P&gt;Maybe you should try another 4GB Scandisk card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 16:24:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SD-Card-support-issues/m-p/1011651#M6503</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-02-14T16:24:17Z</dc:date>
    </item>
  </channel>
</rss>