<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Differences between IMXRT1052 and IMXRT1062 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Differences-between-IMXRT1052-and-IMXRT1062/m-p/1009941#M6385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm developing a project for a IMXRT1062xxx5A using EmbOS. To start it, I took a sample project provided by EmbOS, but since they didn't have a project for my board, I used the one for the IMXRT1052. I searched for information online and I found out that basically the 2 boards are the same except for minor stuff, that's why EmbOS provided only one example valid for both the boards.&lt;/P&gt;&lt;P&gt;However, this leaves me with a couple of doubts about the provided files like "system_MIMXRT105x.c" and "startup_MIMXRT1052.s".&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently able to compile and flash the code without any error, but my questions are:&lt;/P&gt;&lt;P&gt;1) since the IMXRT1062 has more functionalities, are these files enough or should I change/add something?&lt;/P&gt;&lt;P&gt;2) I saw many sample projects for the same board with different structures, some of them have a "board.h" and "board.c" in addition to the two files I mention before, some of them have a really long startup file while others have a really short one... I'm gonna attach my project here, does it have the right structure? do I have the right files? am I missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice is well accepted!&amp;nbsp;&lt;/P&gt;&lt;P&gt;I thank you for your help.&lt;/P&gt;&lt;P&gt;Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Dec 2019 15:54:07 GMT</pubDate>
    <dc:creator>jack__</dc:creator>
    <dc:date>2019-12-04T15:54:07Z</dc:date>
    <item>
      <title>Differences between IMXRT1052 and IMXRT1062</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Differences-between-IMXRT1052-and-IMXRT1062/m-p/1009941#M6385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm developing a project for a IMXRT1062xxx5A using EmbOS. To start it, I took a sample project provided by EmbOS, but since they didn't have a project for my board, I used the one for the IMXRT1052. I searched for information online and I found out that basically the 2 boards are the same except for minor stuff, that's why EmbOS provided only one example valid for both the boards.&lt;/P&gt;&lt;P&gt;However, this leaves me with a couple of doubts about the provided files like "system_MIMXRT105x.c" and "startup_MIMXRT1052.s".&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently able to compile and flash the code without any error, but my questions are:&lt;/P&gt;&lt;P&gt;1) since the IMXRT1062 has more functionalities, are these files enough or should I change/add something?&lt;/P&gt;&lt;P&gt;2) I saw many sample projects for the same board with different structures, some of them have a "board.h" and "board.c" in addition to the two files I mention before, some of them have a really long startup file while others have a really short one... I'm gonna attach my project here, does it have the right structure? do I have the right files? am I missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice is well accepted!&amp;nbsp;&lt;/P&gt;&lt;P&gt;I thank you for your help.&lt;/P&gt;&lt;P&gt;Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 15:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Differences-between-IMXRT1052-and-IMXRT1062/m-p/1009941#M6385</guid>
      <dc:creator>jack__</dc:creator>
      <dc:date>2019-12-04T15:54:07Z</dc:date>
    </item>
    <item>
      <title>Re: Differences between IMXRT1052 and IMXRT1062</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Differences-between-IMXRT1052-and-IMXRT1062/m-p/1009942#M6386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;Hello,&amp;nbsp;Giacomo&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;Unfortunately, I'm not familiar with the EmbOS example projects. For specific questions of these projects, you will need to contact SEGGER support directly.&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;You can also refer to the SDK that we provide. The advantage of this is that we have a specific SDK for the RT1062, however, it doesn't include EmbOS support, but you have AmazonFreeRTOS. You can download the SDK from the following &lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;link&lt;/A&gt;.&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;Regarding your questions, please see my comments below.&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;1) since the IMXRT1062 has more functionalities, are these files enough or should I change/add something?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;I would recommend you to use the files for the RT106x, you can find those on our SDK for the RT1062.&lt;/P&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;2) I saw many sample projects for the same board with different structures, some of them have a "board.h" and "board.c" in addition to the two files I mention before, some of them have a really long startup file while others have a really short one... I'm gonna attach my project here, does it have the right structure? do I have the right files? am I missing something?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P style="margin: 0in; font-size: 12.0pt;"&gt;As mentioned before, I'm not familiar with the EmbOS example projects, for this question you will need to contact directly SEGGER support.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2019 23:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Differences-between-IMXRT1052-and-IMXRT1062/m-p/1009942#M6386</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-12-06T23:24:44Z</dc:date>
    </item>
  </channel>
</rss>