<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic From which memory IMXRT1020 EVK example codes are executed ? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/From-which-memory-IMXRT1020-EVK-example-codes-are-executed/m-p/1005754#M6266</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since IMXRT 1020 is a cross over processor , which is basically a MCU with a extenal memory , How do i know into which external memory is IMXRT1020 EVK Example codes are flashed into and are executed from , in the example code where do i find the settings or is it done with the IDE settings ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anticipating a quick response&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Naren&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jan 2020 10:07:52 GMT</pubDate>
    <dc:creator>narenchandra401</dc:creator>
    <dc:date>2020-01-27T10:07:52Z</dc:date>
    <item>
      <title>From which memory IMXRT1020 EVK example codes are executed ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/From-which-memory-IMXRT1020-EVK-example-codes-are-executed/m-p/1005754#M6266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since IMXRT 1020 is a cross over processor , which is basically a MCU with a extenal memory , How do i know into which external memory is IMXRT1020 EVK Example codes are flashed into and are executed from , in the example code where do i find the settings or is it done with the IDE settings ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anticipating a quick response&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Naren&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2020 10:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/From-which-memory-IMXRT1020-EVK-example-codes-are-executed/m-p/1005754#M6266</guid>
      <dc:creator>narenchandra401</dc:creator>
      <dc:date>2020-01-27T10:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: From which memory IMXRT1020 EVK example codes are executed ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/From-which-memory-IMXRT1020-EVK-example-codes-are-executed/m-p/1005755#M6267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Naren,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SDK examples boot from IS25LP064 64 Mb QSPI Flash. The Flash driver is selected in the properties of the project.&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101660iCC1BD7699FE423BF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;/P&gt;&lt;P&gt;The settings of this memories are located in the located in the flexspi_nor_confg file in the xip folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 16:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/From-which-memory-IMXRT1020-EVK-example-codes-are-executed/m-p/1005755#M6267</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-01-31T16:52:57Z</dc:date>
    </item>
  </channel>
</rss>