<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic j-flash &amp; u-boot in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/j-flash-u-boot/m-p/782839#M604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;BR /&gt;i am a newbie and my target is mcimx6sx-sdb (i.mx 6soloX proc).&lt;BR /&gt;i have need to place u-boot in qspi flash by J-Flash (i have to use "j-link pluse" device only, i can not use mmc/sd or usb-hid) and run it.&lt;BR /&gt;i can see Flash bank 0(QSPI Flash sytarts from 0x70000000 and end at 0x73FFFFFF) and i can load a bin file (but not a imx file, error "Unsupported file type *imx").&lt;BR /&gt;&lt;SPAN&gt;I have seen &lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="340521" data-objecttype="1" href="https://community.nxp.com/thread/340521"&gt;https://community.nxp.com/thread/340521&lt;/A&gt;&lt;SPAN&gt; but i do not understand sense of some things.&lt;/SPAN&gt;&lt;BR /&gt;could you tell me correct way flashing u-boot image onQuadSPA and run it .&lt;BR /&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Nov 2018 13:09:11 GMT</pubDate>
    <dc:creator>o_scherbinin</dc:creator>
    <dc:date>2018-11-20T13:09:11Z</dc:date>
    <item>
      <title>j-flash &amp; u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/j-flash-u-boot/m-p/782839#M604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;BR /&gt;i am a newbie and my target is mcimx6sx-sdb (i.mx 6soloX proc).&lt;BR /&gt;i have need to place u-boot in qspi flash by J-Flash (i have to use "j-link pluse" device only, i can not use mmc/sd or usb-hid) and run it.&lt;BR /&gt;i can see Flash bank 0(QSPI Flash sytarts from 0x70000000 and end at 0x73FFFFFF) and i can load a bin file (but not a imx file, error "Unsupported file type *imx").&lt;BR /&gt;&lt;SPAN&gt;I have seen &lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="340521" data-objecttype="1" href="https://community.nxp.com/thread/340521"&gt;https://community.nxp.com/thread/340521&lt;/A&gt;&lt;SPAN&gt; but i do not understand sense of some things.&lt;/SPAN&gt;&lt;BR /&gt;could you tell me correct way flashing u-boot image onQuadSPA and run it .&lt;BR /&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 13:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/j-flash-u-boot/m-p/782839#M604</guid>
      <dc:creator>o_scherbinin</dc:creator>
      <dc:date>2018-11-20T13:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: j-flash &amp; u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/j-flash-u-boot/m-p/782840#M605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oleg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;qspi programming with jtag is not supported by nxp, may be useful to look on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://forum.segger.com/index.php/Thread/2934-SOLVED-OR-QSPI-flash-programming-on-iMX6SX/" title="https://forum.segger.com/index.php/Thread/2934-SOLVED-OR-QSPI-flash-programming-on-iMX6SX/"&gt;[SOLVED/OR] QSPI flash programming on iMX6SX - J-Link/Flasher related - SEGGER - Forum&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/debugging-using-segger-j-link-jtag/" title="https://boundarydevices.com/debugging-using-segger-j-link-jtag/"&gt;Debugging using Segger J-Link JTAG - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 23:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/j-flash-u-boot/m-p/782840#M605</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-11-20T23:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: j-flash &amp; u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/j-flash-u-boot/m-p/782841#M606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;have a good day Igor&lt;/P&gt;&lt;P&gt;i tried simple method-load uboot image by mfgtool and then save it a as bin file by J-Flash app. I realize that this is an unpromising way if i have to change target device configuration.&lt;BR /&gt;I see only one way - build my own u-boot image and load it to RAM by J-Link then move it to QSPI nor.&lt;BR /&gt;am i right?&lt;BR /&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 08:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/j-flash-u-boot/m-p/782841#M606</guid>
      <dc:creator>o_scherbinin</dc:creator>
      <dc:date>2018-11-21T08:39:20Z</dc:date>
    </item>
  </channel>
</rss>