<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx RT1020 Problem in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT1020-Problem/m-p/996731#M5955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;When any UART input is high at the powering up stage of the IMXRT1020, seems that the MCU cannot run properly (we cannot see 1.1V supplied by the MCU and nothing works). We observed that issue for these cases:&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;- When an active (means it drives its tx pin high) UART/RS232 converter is connected to UART1 (debug console) of IMXRT1020&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;- When we connect RS485 converter to UART2 of IMXRT1020 and the converter drivers rx pin as high&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;When we isolate those pins, MCU runs perfectly, but when any of them is connected while powering up the MCU, MCU does not work.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We haven't specifically tested all other interfaces, if they have also similar problems. Our problem is on these UART interfaces for now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 03 Nov 2019 15:40:56 GMT</pubDate>
    <dc:creator>mustafa_tarhan</dc:creator>
    <dc:date>2019-11-03T15:40:56Z</dc:date>
    <item>
      <title>i.mx RT1020 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT1020-Problem/m-p/996731#M5955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;When any UART input is high at the powering up stage of the IMXRT1020, seems that the MCU cannot run properly (we cannot see 1.1V supplied by the MCU and nothing works). We observed that issue for these cases:&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;- When an active (means it drives its tx pin high) UART/RS232 converter is connected to UART1 (debug console) of IMXRT1020&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;- When we connect RS485 converter to UART2 of IMXRT1020 and the converter drivers rx pin as high&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;When we isolate those pins, MCU runs perfectly, but when any of them is connected while powering up the MCU, MCU does not work.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We haven't specifically tested all other interfaces, if they have also similar problems. Our problem is on these UART interfaces for now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Nov 2019 15:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT1020-Problem/m-p/996731#M5955</guid>
      <dc:creator>mustafa_tarhan</dc:creator>
      <dc:date>2019-11-03T15:40:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx RT1020 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT1020-Problem/m-p/996732#M5956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="336825" data-username="mustafa.tarhan@arroweurope.com" href="https://community.nxp.com/people/mustafa.tarhan@arroweurope.com"&gt;Mustafa TARHAN&lt;/A&gt; ,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This question is the same question in your case 00239039.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; After several round reply, I think you can let our customer check the power up sequence, whether it is the same as this figure:&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92121i176D598C992DFFC0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Any updated information, you can reply me in the case or here.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2019 08:51:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT1020-Problem/m-p/996732#M5956</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-11-05T08:51:09Z</dc:date>
    </item>
  </channel>
</rss>