<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: USB Bulk out packet size problem</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-Bulk-out-packet-size-problem/m-p/990994#M5795</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you check the Table 42-58 in the reference manual you will see that the maximum packet size the endpoint is capable to receive is 1024, if you want to receive transmission greater than this value I will suggest to partition the package.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103248iC842316A58DBD1F4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Feb 2020 22:03:36 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2020-02-07T22:03:36Z</dc:date>
    <item>
      <title>USB Bulk out packet size problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-Bulk-out-packet-size-problem/m-p/990993#M5794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using rt1050 usb_device_cdc_vcom demo and trying to modify&amp;nbsp;HS_CDC_VCOM_BULK_OUT_PACKET_SIZE from&lt;/P&gt;&lt;P&gt;64 to 2048 or larger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It work's fine when the value is set to 1024.&lt;/P&gt;&lt;P&gt;After change it to 2048 , it sucked while transmit data out.&lt;/P&gt;&lt;P&gt;Is there any limitation ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2020 09:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-Bulk-out-packet-size-problem/m-p/990993#M5794</guid>
      <dc:creator>eric_yp_chen</dc:creator>
      <dc:date>2020-02-06T09:20:52Z</dc:date>
    </item>
    <item>
      <title>Re: USB Bulk out packet size problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-Bulk-out-packet-size-problem/m-p/990994#M5795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you check the Table 42-58 in the reference manual you will see that the maximum packet size the endpoint is capable to receive is 1024, if you want to receive transmission greater than this value I will suggest to partition the package.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103248iC842316A58DBD1F4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2020 22:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-Bulk-out-packet-size-problem/m-p/990994#M5795</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-02-07T22:03:36Z</dc:date>
    </item>
  </channel>
</rss>