<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックQuestion about Using HyperRam and HyperFlash</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-Using-HyperRam-and-HyperFlash/m-p/971681#M4808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have some problems developing an I.MX 1052 application. I need more GPIOs, and flash speed is critical. so I'm thinking about using HyperRam and HyperFlash instead of QSPI Flash and SDRAM. Is it posssible to mount both HyperRam and HyperFlash&amp;nbsp;simultaneously on one flexSPI instance, and XIP boot from HyperFlash? If I do so, will the access speed drop when accessing RAM and FLASH together?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 26 Oct 2019 08:29:57 GMT</pubDate>
    <dc:creator>ChekhovMark</dc:creator>
    <dc:date>2019-10-26T08:29:57Z</dc:date>
    <item>
      <title>Question about Using HyperRam and HyperFlash</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-Using-HyperRam-and-HyperFlash/m-p/971681#M4808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have some problems developing an I.MX 1052 application. I need more GPIOs, and flash speed is critical. so I'm thinking about using HyperRam and HyperFlash instead of QSPI Flash and SDRAM. Is it posssible to mount both HyperRam and HyperFlash&amp;nbsp;simultaneously on one flexSPI instance, and XIP boot from HyperFlash? If I do so, will the access speed drop when accessing RAM and FLASH together?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Oct 2019 08:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-Using-HyperRam-and-HyperFlash/m-p/971681#M4808</guid>
      <dc:creator>ChekhovMark</dc:creator>
      <dc:date>2019-10-26T08:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: Question about Using HyperRam and HyperFlash</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-Using-HyperRam-and-HyperFlash/m-p/971682#M4809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="350346" data-username="1170100305@stu.hit.edu.cn" href="https://community.nxp.com/people/1170100305@stu.hit.edu.cn"&gt;Chekhov Mark&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1)&amp;nbsp; Is it possible to mount both HyperRam and HyperFlash simultaneously on one FlexSPI instance, and XIP boot from HyperFlash?&lt;BR /&gt;-- No, I'm afraid not.&lt;BR /&gt;For the MIMXRT1052, it's capable of working with the HyperRam and HyperFlash simultaneously, as it has the FlexSPI A and FlexSPI B.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/93788iD6F763B9F07E06D4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2019 02:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-Using-HyperRam-and-HyperFlash/m-p/971682#M4809</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-10-29T02:02:12Z</dc:date>
    </item>
  </channel>
</rss>