<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What kind of reset is triggered by the POR_B pin? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970772#M4784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Kerry Zhou wrote:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;Actually, the MIMXRT1050-EVKB board also use the reset button connect to the POR_b, I have test the code, when debug, if press the reset button, the debugger will be disconnect, so you can consider it as POR.&lt;/BLOCKQUOTE&gt;&lt;P&gt;This is not correct. It looks like you've never seen the EVKB schematics. Have you ever really worked on it or do you speak by hearsay?&lt;/P&gt;&lt;P&gt;On the EVKB the POR_BUTTON is &lt;STRONG&gt;NOT&lt;/STRONG&gt; directly connected to POR_B pin:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="evkb_por_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85979iF3A18E9D226FE18D/image-size/large?v=v2&amp;amp;px=999" role="button" title="evkb_por_1.png" alt="evkb_por_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the POR_BUTTON it is connected to pin MR of the power supply monitor U5, which in turn removes the enable to the DCDC converter U3. So the DCDC_3V3 is turned off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="evkb_por_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85980iE565961CBDBFA1E1/image-size/large?v=v2&amp;amp;px=999" role="button" title="evkb_por_2.png" alt="evkb_por_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the DCDC_3V3 is turned off, the U2 power monitor asserts a reset that it is connected directly to the POR_B pin of the microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The POR_B pin of the micro is then connected to the JTAG J21 connectors and to the J25 connector.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="evkb_por_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85981iC525660C602610B5/image-size/large?v=v2&amp;amp;px=999" role="button" title="evkb_por_3.png" alt="evkb_por_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So if you tried by pressing the POR_BUTTON SW3 button, you caused a power failure, and then a powerup sequence as described in the reference manual. In this case it can be explained so that the JTAG disconnects. In summary, it is true that pressing POR_BUTTON causes the assertion of the POR_B signal on the micro, but as an indirect consequence of the power supply drop DCDC_3V3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The case I would like to clarify is to drive low the POR_B pin without turning off the DCDC_3V3 power supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I encourage you to try using the signal from the J25 connector (obviously closing the J26 jumper). Does the JTAG disconnect in this case or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jun 2019 07:45:39 GMT</pubDate>
    <dc:creator>mastupristi</dc:creator>
    <dc:date>2019-06-12T07:45:39Z</dc:date>
    <item>
      <title>What kind of reset is triggered by the POR_B pin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970770#M4782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm referring to RT1051.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on the Reference Manual (page 1242/1243):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="reset.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85890iD4130D9912DCAA65/image-size/large?v=v2&amp;amp;px=999" role="button" title="reset.png" alt="reset.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So the Cold reset does not reset all the peripherals, unlike the POR reset.&lt;/P&gt;&lt;P&gt;The name of the POR (&lt;STRONG&gt;PowerOn Reset&lt;/STRONG&gt;) reset makes me think that it can only be triggered when the micro is powered. Is that right?&lt;/P&gt;&lt;P&gt;What happens if I assert the POR_B signal (is pulled down) when the power supplies are already on and stable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the Datasheet I found (page 16):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="cold.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85891i7692C55B345BF685/image-size/large?v=v2&amp;amp;px=999" role="button" title="cold.png" alt="cold.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the POR_B signal cause a cold reset or a POR reset?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 08:02:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970770#M4782</guid>
      <dc:creator>mastupristi</dc:creator>
      <dc:date>2019-06-11T08:02:53Z</dc:date>
    </item>
    <item>
      <title>Re: What kind of reset is triggered by the POR_B pin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970771#M4783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;STRONG&gt;&lt;A _jive_internal="true" data-avatarid="-1" data-content-finding="Community" data-userid="266483" data-username="mastupristi" href="https://community.nxp.com/people/mastupristi"&gt;Massimiliano Cialdi&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check these information from the reference manual:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_14.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85962i1702BDFCCB8FB320/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_14.png" alt="pastedImage_14.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_15.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85972i92EB05D4B9AE61F2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_15.png" alt="pastedImage_15.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the POR_B is used to reset the entire chip including test logic and JTAG modules.&lt;/P&gt;&lt;P&gt;Then you can consider the POR_B as the POR reset.&lt;/P&gt;&lt;P&gt;Actually, the MIMXRT1050-EVKB board also use the reset button connect to the POR_b, I have test the code, when debug, if press the reset button, the debugger will be disconnect, so you can consider it as POR.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 06:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970771#M4783</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-06-12T06:07:51Z</dc:date>
    </item>
    <item>
      <title>Re: What kind of reset is triggered by the POR_B pin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970772#M4784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Kerry Zhou wrote:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;Actually, the MIMXRT1050-EVKB board also use the reset button connect to the POR_b, I have test the code, when debug, if press the reset button, the debugger will be disconnect, so you can consider it as POR.&lt;/BLOCKQUOTE&gt;&lt;P&gt;This is not correct. It looks like you've never seen the EVKB schematics. Have you ever really worked on it or do you speak by hearsay?&lt;/P&gt;&lt;P&gt;On the EVKB the POR_BUTTON is &lt;STRONG&gt;NOT&lt;/STRONG&gt; directly connected to POR_B pin:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="evkb_por_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85979iF3A18E9D226FE18D/image-size/large?v=v2&amp;amp;px=999" role="button" title="evkb_por_1.png" alt="evkb_por_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the POR_BUTTON it is connected to pin MR of the power supply monitor U5, which in turn removes the enable to the DCDC converter U3. So the DCDC_3V3 is turned off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="evkb_por_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85980iE565961CBDBFA1E1/image-size/large?v=v2&amp;amp;px=999" role="button" title="evkb_por_2.png" alt="evkb_por_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the DCDC_3V3 is turned off, the U2 power monitor asserts a reset that it is connected directly to the POR_B pin of the microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The POR_B pin of the micro is then connected to the JTAG J21 connectors and to the J25 connector.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="evkb_por_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85981iC525660C602610B5/image-size/large?v=v2&amp;amp;px=999" role="button" title="evkb_por_3.png" alt="evkb_por_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So if you tried by pressing the POR_BUTTON SW3 button, you caused a power failure, and then a powerup sequence as described in the reference manual. In this case it can be explained so that the JTAG disconnects. In summary, it is true that pressing POR_BUTTON causes the assertion of the POR_B signal on the micro, but as an indirect consequence of the power supply drop DCDC_3V3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The case I would like to clarify is to drive low the POR_B pin without turning off the DCDC_3V3 power supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I encourage you to try using the signal from the J25 connector (obviously closing the J26 jumper). Does the JTAG disconnect in this case or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 07:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970772#M4784</guid>
      <dc:creator>mastupristi</dc:creator>
      <dc:date>2019-06-12T07:45:39Z</dc:date>
    </item>
    <item>
      <title>Re: What kind of reset is triggered by the POR_B pin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970773#M4785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Max,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks a lot for your detail reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Yes, I have tested the J26_1, and connect it to GND, this is the result:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86009i8BCDF3E8DD9941A6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You can find the debugger is stopped after the POR_b connect to GND.&lt;/P&gt;&lt;P&gt;&amp;nbsp;If you still have any question about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 09:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-kind-of-reset-is-triggered-by-the-POR-B-pin/m-p/970773#M4785</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-06-12T09:52:26Z</dc:date>
    </item>
  </channel>
</rss>