<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: i.MXRT1060 ADC external trigger (ADC_ETC) for ADC 2</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963754#M4641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jeremyzhou,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found my problem. Turns out I had to use XBAR1, instead of XBAR0, to trigger ADC2. I couldn't find anything on the documentation about that, so I had to guess and try. It works now.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Cedric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Oct 2019 13:30:39 GMT</pubDate>
    <dc:creator>cedric1</dc:creator>
    <dc:date>2019-10-11T13:30:39Z</dc:date>
    <item>
      <title>i.MXRT1060 ADC external trigger (ADC_ETC) for ADC 2</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963752#M4639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two instance of ADC in i.MXRT1060. I can make ADC 1 work with external trigger on pin J11 GPIO_AD_B1_00 using ADC channel 5. This pin can also work with ADC 2. I can make ADC 2 work fine when using software trigger, but I can't make it work with external trigger. I think it has something to do with the TSC. I did try to&amp;nbsp;set&amp;nbsp;ADC_ETC.TSC_BYPASS and&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;ADC_ETC.EXT0_TRIG_ENABLE. Any idea why I can't make ADC 2 work with ADC_ETC on this pin?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Cedric&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 21:00:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963752#M4639</guid>
      <dc:creator>cedric1</dc:creator>
      <dc:date>2019-10-09T21:00:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1060 ADC external trigger (ADC_ETC) for ADC 2</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963753#M4640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="347977" data-username="cedric@rmds.ca" href="https://community.nxp.com/people/cedric@rmds.ca"&gt;Cédric Lemay&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;I'd like to gather more information about your implementation, &lt;BR /&gt;so whether you can introduce the steps you did, especial the code parts.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 10:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963753#M4640</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-10-11T10:50:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1060 ADC external trigger (ADC_ETC) for ADC 2</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963754#M4641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jeremyzhou,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found my problem. Turns out I had to use XBAR1, instead of XBAR0, to trigger ADC2. I couldn't find anything on the documentation about that, so I had to guess and try. It works now.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Cedric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 13:30:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963754#M4641</guid>
      <dc:creator>cedric1</dc:creator>
      <dc:date>2019-10-11T13:30:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1060 ADC external trigger (ADC_ETC) for ADC 2</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963755#M4642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="347977" data-objecttype="3" href="https://community.nxp.com/people/cedric@rmds.ca"&gt;Cédric Lemay&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thanks for your reply and I'm glad to hear the problem is solved.&lt;BR /&gt;According to your reply, whether it means tha you need to use the XBAR1(XBARA), the XBAR2 and XBARB (XBARB) is unavailable.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2019 02:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1060-ADC-external-trigger-ADC-ETC-for-ADC-2/m-p/963755#M4642</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-10-14T02:01:24Z</dc:date>
    </item>
  </channel>
</rss>