<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1064 Serial Loader in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-Serial-Loader/m-p/961846#M4594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently purchased MIMXRT1064-EVK and I realize that an additional LPC4322JET100 MCU is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a new board and I need a USB programming port. I do not require any other debugging tools.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I directly connect D+ and D- of the USB to my USB port of MIMXRT1064 instead of going through an additional MCU?&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;Can I use my UART port instead?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jul 2019 08:06:26 GMT</pubDate>
    <dc:creator>klinsmann_mah5</dc:creator>
    <dc:date>2019-07-24T08:06:26Z</dc:date>
    <item>
      <title>MIMXRT1064 Serial Loader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-Serial-Loader/m-p/961846#M4594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently purchased MIMXRT1064-EVK and I realize that an additional LPC4322JET100 MCU is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a new board and I need a USB programming port. I do not require any other debugging tools.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I directly connect D+ and D- of the USB to my USB port of MIMXRT1064 instead of going through an additional MCU?&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;Can I use my UART port instead?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2019 08:06:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-Serial-Loader/m-p/961846#M4594</guid>
      <dc:creator>klinsmann_mah5</dc:creator>
      <dc:date>2019-07-24T08:06:26Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 Serial Loader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-Serial-Loader/m-p/961847#M4595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="338176" data-username="klinsmann_mah5@hotmail.com" href="https://community.nxp.com/people/klinsmann_mah5@hotmail.com"&gt;KLINSMANN MAH&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Can I use my UART port instead?&lt;BR /&gt;-- Yes, you can.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 01:19:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1064-Serial-Loader/m-p/961847#M4595</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-07-25T01:19:29Z</dc:date>
    </item>
  </channel>
</rss>