<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: Firmware Update</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950923#M4279</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Sagar Prajapati &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;You can enable serial download by default out of reset and after every power-on reset, it will boot from the ROM code with HID interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jul 2019 19:30:27 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-07-16T19:30:27Z</dc:date>
    <item>
      <title>Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950918#M4274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to use secondary bootloader in IMX RT 1064 development board with default configuration in IAR Embedded Workbench. I have tried using SDK example by changing the linker file.Firmware is boot from QSPI Flash.BL_TARGET_RAM is defined as preprocessor. Will you please give some working example?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jul 2019 11:10:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950918#M4274</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2019-07-06T11:10:09Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950919#M4275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sagar Prajapati&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, as you mentioned, the secondary bootloader that we provide with the mcuboot is a RAM bootloader, and unfortunately, at the moment there isn't a flash resident bootloader for the RT families, you can implement this application, but you will need to place the "erase/write" code in the internal ram.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jive_macro_thread jive_macro link-titled" data-orig-content="Using QSPI Flash on imxrt1060 EVK for booting and back-up storage" href="https://community.nxp.com/thread/486654" title="Using QSPI Flash on imxrt1060 EVK for booting and back-up storage"&gt;Using QSPI Flash on imxrt1060 EVK for booting and back-up storage&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jive_macro_thread jive_macro link-titled" data-orig-content="RT1050 QSPI Flash Limitations" href="https://community.nxp.com/thread/464926" title="RT1050 QSPI Flash Limitations"&gt;RT1050 QSPI Flash Limitations&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 23:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950919#M4275</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-07-09T23:39:09Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950920#M4276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;Then what is the procedure to update firmware in field without debugger?Regards,SagarFrom: jorge_a_vazquez &amp;amp;lt;admin@community.nxp.com&amp;amp;gt;Sent: Wed, 10 Jul 2019 05:10:32 GMT+0530To: Sagar Prajapati &amp;amp;lt;sagar.prajapati@mantratec.com&amp;amp;gt;Subject: Re:  - Firmware Update&amp;nbsp;																														NXP Community 																		&lt;/P&gt;&lt;P&gt;																								Re: Firmware Update&lt;/P&gt;&lt;P&gt;						reply from Jorge Antonio Alcala Vazquez in i.MX RT - View the full discussion&lt;/P&gt;&lt;P&gt;																								Hi Sagar Prajapati&lt;/P&gt;&lt;P&gt;						&amp;nbsp;&lt;/P&gt;&lt;P&gt;						Yes, as you mentioned, the secondary bootloader that we provide with the mcuboot is a RAM bootloader, and unfortunately, at the moment there isn&amp;amp;#39;t a flash resident bootloader for the RT families, you can implement this application, but you will need to place the &amp;amp;quot;erase/write&amp;amp;quot; code in the internal ram.&lt;/P&gt;&lt;P&gt;						&amp;nbsp;&lt;/P&gt;&lt;P&gt;						Using QSPI Flash on imxrt1060 EVK for booting and back-up storage&amp;nbsp;&lt;/P&gt;&lt;P&gt;						RT1050 QSPI Flash Limitations&amp;nbsp;&lt;/P&gt;&lt;P&gt;						&amp;nbsp;&lt;/P&gt;&lt;P&gt;						Hope this helps.						Have a great day,						TIC&lt;/P&gt;&lt;P&gt;						&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2019 13:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950920#M4276</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2019-07-11T13:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950921#M4277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Sagar Prajapati &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;If you enable USB or UART, you can use the ROM code that is in the RT10xx families, this code can be used along with the mfgtool tool or with the MCUbootutility to program your external memory.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;A _jive_internal="true" class="jive_macro jive_macro_document link-titled" href="https://community.nxp.com/docs/DOC-343447" title="One-stop secure boot tool: NXP-MCUBootUtility is upgraded to v1.4.0"&gt;One-stop secure boot tool: NXP-MCUBootUtility is upgraded to v1.4.0&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hope this helps&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2019 15:26:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950921#M4277</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-07-11T15:26:01Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950922#M4278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But for this functionality, every time we need to enable serial download boot mode using switch. For custom hardware it is not proper way. We need something like ROM bootloader like after every power on reset it boots and coming in HID devices. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2019 03:36:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950922#M4278</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2019-07-15T03:36:39Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950923#M4279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Sagar Prajapati &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;You can enable serial download by default out of reset and after every power-on reset, it will boot from the ROM code with HID interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 19:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950923#M4279</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-07-16T19:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950924#M4280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello jorge,Can you please share related document and procedure to enable this feature?RegardsSagarFrom: jorge_a_vazquez &amp;amp;lt;admin@community.nxp.com&amp;amp;gt;Sent: Wed, 17 Jul 2019 01:00:48 GMT+0530To: Sagar Prajapati &amp;amp;lt;sagar.prajapati@mantratec.com&amp;amp;gt;Subject: Re:  - Firmware Update&amp;nbsp;																														NXP Community 																		&lt;/P&gt;&lt;P&gt;																								Re: Firmware Update&lt;/P&gt;&lt;P&gt;						reply from Jorge Antonio Alcala Vazquez in i.MX RT - View the full discussion&lt;/P&gt;&lt;P&gt;																								Hi Sagar Prajapati &lt;/P&gt;&lt;P&gt;						&amp;nbsp;&lt;/P&gt;&lt;P&gt;						You can enable serial download by default out of reset and after every power-on reset, it will boot from the ROM code with HID interface.&lt;/P&gt;&lt;P&gt;						&amp;nbsp;&lt;/P&gt;&lt;P&gt;						Regards												&lt;/P&gt;&lt;P&gt;																														Reply to this message by replying to this email, or go to the message on NXP Community																									Start a new discussion in i.MX RT by email or at NXP Community																									Following Re: Firmware Update in these streams: Inbox																					&lt;/P&gt;&lt;P&gt;						This email was sent by NXP Community because you are a registered user.						You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences																								s&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This email and any files transmitted with it are confidential and intended solely for the use of the individual or entity to whom they are addressed. If you are not the named addressee you should not disseminate, distribute or copy this e-mail. Please notify the sender immediately by e-mail if you have received this e-mail by mistake and delete this e-mail from your system.Â&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 03:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950924#M4280</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2019-07-17T03:45:59Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950925#M4281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Sagar Prajapati &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;If you mean how to enable the boot from the ROM code, it can be done with the GPIO (boot from GPIO) or you can use the boot from the fuses, so every time you have a reset, it will boot from the ROM code.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 15:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Firmware-Update/m-p/950925#M4281</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-07-17T15:26:36Z</dc:date>
    </item>
  </channel>
</rss>