<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question about creating bootable image for FlexSPINOR XIP for IMXRT1052 (again) in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948406#M4206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I am missing something fundamental in the process of creating a bootable image using the elftosb utility.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am getting confused on the right steps to use an .srec (s19) file directly from an MCUXpresso .axf file.&amp;nbsp; I assume I can use a build with XIP_BOOT_HEADER_ENABLE=1 and XIP_EXTERNAL_FLASH=1&amp;nbsp; if the .bd file is not specifying a dcd.bin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also not sure why the documentation instructs to change the FLASH region from 0x60000000 to 0x60002000.&amp;nbsp; Is this necessary if XIP_BOOT_HEADER_ENABLE=1 and dcd.bin isn't used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The default bd file included with elftosb has the dcd file commented out (imx-flexspinor-normal-unsigned.bd)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I am trying to get the build process down to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Compile (example) project as-is for XIP&amp;nbsp;&amp;nbsp; (FLASH at 0x60000000, XIP_BOOT_HEADER_ENABLE=1 , XIP_EXTERNAL_FLASH=1), not Linked to RAM.&lt;/P&gt;&lt;P&gt;2. Generate .srec (s19) file from MCUXpresso&lt;/P&gt;&lt;P&gt;3. Use elftosb with the generated .srec and default imx-flexspinor-normal-unsigned.bd&amp;nbsp; (no dcd.bin) to generate bootable image (.bin)&lt;/P&gt;&lt;P&gt;4. Use blhost to upload .bin to flash using flashloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Aug 2019 15:04:34 GMT</pubDate>
    <dc:creator>jackking</dc:creator>
    <dc:date>2019-08-20T15:04:34Z</dc:date>
    <item>
      <title>Question about creating bootable image for FlexSPINOR XIP for IMXRT1052 (again)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948406#M4206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I am missing something fundamental in the process of creating a bootable image using the elftosb utility.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am getting confused on the right steps to use an .srec (s19) file directly from an MCUXpresso .axf file.&amp;nbsp; I assume I can use a build with XIP_BOOT_HEADER_ENABLE=1 and XIP_EXTERNAL_FLASH=1&amp;nbsp; if the .bd file is not specifying a dcd.bin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also not sure why the documentation instructs to change the FLASH region from 0x60000000 to 0x60002000.&amp;nbsp; Is this necessary if XIP_BOOT_HEADER_ENABLE=1 and dcd.bin isn't used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The default bd file included with elftosb has the dcd file commented out (imx-flexspinor-normal-unsigned.bd)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I am trying to get the build process down to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Compile (example) project as-is for XIP&amp;nbsp;&amp;nbsp; (FLASH at 0x60000000, XIP_BOOT_HEADER_ENABLE=1 , XIP_EXTERNAL_FLASH=1), not Linked to RAM.&lt;/P&gt;&lt;P&gt;2. Generate .srec (s19) file from MCUXpresso&lt;/P&gt;&lt;P&gt;3. Use elftosb with the generated .srec and default imx-flexspinor-normal-unsigned.bd&amp;nbsp; (no dcd.bin) to generate bootable image (.bin)&lt;/P&gt;&lt;P&gt;4. Use blhost to upload .bin to flash using flashloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Aug 2019 15:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948406#M4206</guid>
      <dc:creator>jackking</dc:creator>
      <dc:date>2019-08-20T15:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: Question about creating bootable image for FlexSPINOR XIP for IMXRT1052 (again)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948407#M4207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="310308" data-username="jackking" href="https://community.nxp.com/people/jackking"&gt;Jack King&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I'd highly recommend you refer to the &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-341317"&gt;post&lt;/A&gt; which illustrates the process to generate a boot image for Hyperflash.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2019 02:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948407#M4207</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-08-21T02:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: Question about creating bootable image for FlexSPINOR XIP for IMXRT1052 (again)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948408#M4208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As always, thanks for the help.&lt;/P&gt;&lt;P&gt;I am already using that post as a guide for the process.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That post doesn't explain *why* you must set the flash region to 0x60002000...&amp;nbsp; is it to leave room for the dcd block?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That post also seems to assume the .bd file has dcd.bin defined, but the default .bd file included with MFGtools has the dcd file commented out, and there isn't a "-dcd" version of the bd file.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I leave the XIP_BOOT_HEADER_ENABLE=1, I assume dcd.bin isn't needed and I leave the flash region at 0x60000000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2019 02:41:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948408#M4208</guid>
      <dc:creator>jackking</dc:creator>
      <dc:date>2019-08-21T02:41:36Z</dc:date>
    </item>
    <item>
      <title>Re: Question about creating bootable image for FlexSPINOR XIP for IMXRT1052 (again)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948409#M4209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="310308" data-objecttype="3" href="https://community.nxp.com/people/jackking"&gt;Jack King&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;BR /&gt;1) That post doesn't explain *why* you must set the flash region to 0x60002000...&amp;nbsp; is it to leave room for the dcd block?&lt;BR /&gt;-- No, it's used to leave room for the area be highlighted by the red rectangle.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88764i766953D5DE54C076/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2019 06:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948409#M4209</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-08-21T06:51:24Z</dc:date>
    </item>
    <item>
      <title>Re: Question about creating bootable image for FlexSPINOR XIP for IMXRT1052 (again)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948410#M4210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the further details.&amp;nbsp; How does that block get added to the image when using MCUXpresso directly with a debugger (J-Link), and why is it not possible to create a bootable image directly from MCUXpresso?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I think part of my problem is that I am Mac.&amp;nbsp; I pulled the elftosb for Mac from the NXP-MCUBootUtility package, but it looks like this utility isn't ready for use (it generates a1.6GB .bin file from my .srec!).&amp;nbsp;&amp;nbsp; If I use the Windows version of elftosb, it seems to function as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 15:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948410#M4210</guid>
      <dc:creator>jackking</dc:creator>
      <dc:date>2019-08-22T15:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: Question about creating bootable image for FlexSPINOR XIP for IMXRT1052 (again)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948411#M4211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="310308" data-objecttype="3" href="https://community.nxp.com/people/jackking"&gt;Jack King&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;BR /&gt;1) How does that block gets added to the image when using MCUXpresso directly with a debugger (J-Link)?&lt;BR /&gt;-- Go to C/C++ Build &amp;gt;&amp;gt;settings &amp;gt; MCU C compiler &amp;gt; preprocessor and set the XIP_boot_header enable and and XIP_boot_header_DCD_enable both to 1 if you have a dcd.bin file to use. &lt;BR /&gt;1) Why is it not possible to create a bootable image directly from MCUXpresso?&lt;BR /&gt;-- The elftosb is an independent tool and not integrated into the MCUXpresso IDE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2019 03:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-creating-bootable-image-for-FlexSPINOR-XIP-for/m-p/948411#M4211</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-08-23T03:08:57Z</dc:date>
    </item>
  </channel>
</rss>