<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1064 programming the internal Flash at the same time as using HyperRAM in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948374#M4201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The QSPI NOR Flash driver is not located in the on-chip ROM, it is the part of the MCUXpresso SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, the issue mostly looks like the bug in the driver. So, you have to check/debug the driver code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my side, I can try to escalate the issue to R&amp;amp;D, but the fast bug fix is not guaranteed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jun 2019 07:43:53 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2019-06-27T07:43:53Z</dc:date>
    <item>
      <title>RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948371#M4198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have come to a tiresome problem in one of our projects.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The system uses a RT1064, HyperRAM (8 Mbyte) and the code runs out of the internal 4 MByte Flash in the 1064.&lt;/P&gt;&lt;P&gt;The HyperRAM is connected to FlexSPI and the internal Flash is by nature, connected to FlexSPI2.&lt;/P&gt;&lt;P&gt;In my bootloader, I need to have access to the HyperRAM at the same time as programming the internal Flash. This seems not to be possible ??&lt;/P&gt;&lt;P&gt;I can program the internal flash just fine using the NOR Flash driver in the device, but as soon as I do:&lt;/P&gt;&lt;P&gt;status = flexspi_nor_flash_init(instance, &amp;amp;config); // instance is 1 in this case&lt;/P&gt;&lt;P&gt;I loose the connection to the HyperRAM.&lt;/P&gt;&lt;P&gt;Is that to be expected, and more importantly, is there a way around it ?&lt;/P&gt;&lt;P&gt;In this particular case I need to load a firmware file from a filesystem and program that to the internal Flash.&lt;/P&gt;&lt;P&gt;(I'm using the internal 1 MB SRAM for other purposes (filesystem etc etc) so its not an option to use that)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When debugging, I can see that as soon as the NOR Flash driver is called for the internal Flash on FlexSPI2, the FlexSPI is also affected, most of its registers are set to 0. This seems strange as I specifically asks for FlexSPI2 which should be for the internal Flash (or is that determined by the address space)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 12:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948371#M4198</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2019-06-19T12:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948372#M4199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To make the situation more clear, please specify the following: where your code runs from when you try to initialize the NOR Flash for write? Is it XiP from HyperRAM on FlexSPI, or XiP from QSPI NOR Flash on FlexSPI2, or is it internal RAM? In case of XiP from QSPI NOR Flash on FlexSPI2, the situation is clear and the answer is: there is no way to XiP from a QSPI NOR Flash and write to the same Flash at the same time.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 10:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948372#M4199</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-06-26T10:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948373#M4200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&amp;nbsp;Arthur.&lt;/P&gt;&lt;P&gt;The code runs from XIP (internal NOR Flash of the RT1064 on FlexSPI2 at 0x70000000). The HyperRAM is connected to FlexSPI (at 0x60000000).&lt;/P&gt;&lt;P&gt;I use the Flash NOR drivers of the chip (I assume they are in ROM). This works perfectly fine, I can program the Flash without problems.&lt;/P&gt;&lt;P&gt;The "only" issue is that when the ROM driver function&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;flexspi_nor_flash_init(instance, &amp;amp;config); is called (to start the programming access to the internal NOR Flash) I loose connection to the HyperRAM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The strange thing is that the internal Flash and the HyperRAM is on seperate FlexSPI busses, but nevertheless, when I access the Flash on FlexSPI2, the HyperRAM on FlexSPI is failing.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;After the Flash access (after I update my main firmware), I need to init the HyperRAM again to re-gain access to it (contents are destroyed).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hope this makes it clear ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 12:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948373#M4200</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2019-06-26T12:02:42Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948374#M4201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The QSPI NOR Flash driver is not located in the on-chip ROM, it is the part of the MCUXpresso SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, the issue mostly looks like the bug in the driver. So, you have to check/debug the driver code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my side, I can try to escalate the issue to R&amp;amp;D, but the fast bug fix is not guaranteed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2019 07:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948374#M4201</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-06-27T07:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948375#M4202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the code I use:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// IAP.c               20190329 CHG&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// See section 8.13.2 in RTR1064 Users Manual regarding FlexSPI NOR API&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"System.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_flexspi.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_rtwdog.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_wdog.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"evkmimxrt1064_flexspi_nor_config.h"&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;// Contains definition of flexspi_nor_config_t etc&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"IAP.h"&lt;/SPAN&gt;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;typedef&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_GetDefaultConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rtwdog_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_Init&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; rtwdog_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_Deinit&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_Enable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_Disable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_EnableInterrupts&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t mask&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_DisableInterrupts&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t mask&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 uint32_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_GetStatusFlags&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_ClearStatusFlags&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t mask&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_SetTimeoutValue&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint16_t timeoutCount&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_SetWindowValue&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint16_t windowValue&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_Unlock&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_Refresh&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 uint16_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;RTWDOG_GetCounterValue&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;RTWDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; rtwdog_driver_interface_t&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;typedef&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_GetDefaultConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;wdog_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_Init&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; wdog_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_Deinit&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_Enable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_Disable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_EnableInterrupts&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint16_t mask&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 uint16_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_GetStatusFlags&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_ClearInterruptStatus&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint16_t mask&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_SetTimeoutValue&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint16_t timeoutCount&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_SetInterrputTimeoutValue&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint16_t timeoutCount&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_DisablePowerDownEnable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;WDOG_Refresh&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;WDOG_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; wdog_driver_interface_t&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;typedef&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; _serial_nor_config_option &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;union&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
   uint32_t max_freq &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Maximum supported Frequency&lt;/SPAN&gt;
   uint32_t misc_mode &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; miscellaneous mode&lt;/SPAN&gt;
   uint32_t quad_mode_setting &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Quad mode setting&lt;/SPAN&gt;
   uint32_t cmd_pads &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Command pads&lt;/SPAN&gt;
   uint32_t query_pads &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; SFDP read pads&lt;/SPAN&gt;
   uint32_t device_type &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Device type&lt;/SPAN&gt;
   uint32_t option_size &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Option size, in terms of uint32_t, size = (option_size + 1) * 4&lt;/SPAN&gt;
   uint32_t tag &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Tag, must be 0x0E&lt;/SPAN&gt;
  &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; B&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  uint32_t U&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; option0&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;union&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
   uint32_t dummy_cycles &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Dummy cycles before read&lt;/SPAN&gt;
   uint32_t reserved0 &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Reserved for future use&lt;/SPAN&gt;
   uint32_t pinmux_group &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; The pinmux group selection&lt;/SPAN&gt;
   uint32_t reserved1 &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Reserved for future use&lt;/SPAN&gt;
   uint32_t flash_connection &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Flash connection option: 0 - Single Flash connected to port A&lt;/SPAN&gt;
  &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; B&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  uint32_t U&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; option1&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; serial_nor_config_option_t&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;


&lt;SPAN class="keyword token"&gt;typedef&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;enum&lt;/SPAN&gt; _FlexSPIOperationType &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 kFlexSpiOperation_Command&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; FlexSPI operation: Only command, both TX and RX buffer are ignored.&lt;/SPAN&gt;
 kFlexSpiOperation_Config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; FlexSPI operation: Configure device mode, the TX FIFO size is fixed in LUT.&lt;/SPAN&gt;
 kFlexSpiOperation_Write&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; FlexSPI operation: Write, only TX buffer is effective&lt;/SPAN&gt;
 kFlexSpiOperation_Read&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; FlexSPI operation: Read, only Rx Buffer is effective.&lt;/SPAN&gt;
 kFlexSpiOperation_End &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kFlexSpiOperation_Read&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; flexspi_operation_t&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;typedef&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; _FlexSpiXfer &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 flexspi_operation_t operation&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; FlexSPI operation&lt;/SPAN&gt;
 uint32_t baseAddress&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; FlexSPI operation base address&lt;/SPAN&gt;
 uint32_t seqId&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Sequence Id&lt;/SPAN&gt;
 uint32_t seqNum&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Sequence Number&lt;/SPAN&gt;
 bool isParallelModeEnable&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Is a parallel transfer&lt;/SPAN&gt;
 uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;txBuffer&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Tx buffer&lt;/SPAN&gt;
 uint32_t txSize&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Tx size in bytes&lt;/SPAN&gt;
 uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;rxBuffer&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Rx buffer&lt;/SPAN&gt;
 uint32_t rxSize&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Rx size in bytes&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; flexspi_xfer_t&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;


&lt;SPAN class="keyword token"&gt;typedef&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 uint32_t version&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;init&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;program&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t dst_addr&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;src&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;erase_all&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;erase&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t start&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t lengthInBytes&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;read&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;dst&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t addr&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t lengthInBytes&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;clear_cache&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;xfer&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_xfer_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;xfer&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;update_lut&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t seqIndex&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;lutBase&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t seqNumber&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 status_t &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;get_config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; serial_nor_config_option_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;option&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; flexspi_nor_driver_interface_t&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;typedef&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t version&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Bootloader version number&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;copyright&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Bootloader Copyright&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;runBootloader&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;arg&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Function to start the bootloader executing&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;reserved0&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Reserved&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; flexspi_nor_driver_interface_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; FlexSPI NOR Flash API&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;reserved1&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//!&amp;lt; Reserved&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; rtwdog_driver_interface_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;rtwdogDriver&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; wdog_driver_interface_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;wdogDriver&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;reserved2&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; bootloader_api_entry_t&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define g_bootloaderTree (*(bootloader_api_entry_t**)(0x0020001c))&lt;/SPAN&gt;








&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
status_t &lt;SPAN class="token function"&gt;flexspi_nor_flash_init&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; g_bootloaderTree&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;init&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
status_t &lt;SPAN class="token function"&gt;flexspi_nor_flash_page_program&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t dstAddr&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;src&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; g_bootloaderTree&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;program&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; dstAddr&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; src&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
status_t &lt;SPAN class="token function"&gt;flexspi_nor_flash_erase_all&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; g_bootloaderTree&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;erase_all&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
status_t &lt;SPAN class="token function"&gt;flexspi_nor_get_config&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; serial_nor_config_option_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;option&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; g_bootloaderTree&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;get_config&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; option&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
status_t &lt;SPAN class="token function"&gt;flexspi_nor_flash_erase&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t start&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t length&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; g_bootloaderTree&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;erase&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; start&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; length&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
status_t &lt;SPAN class="token function"&gt;flexspi_nor_flash_read&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; flexspi_nor_config_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;dst&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t start&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; uint32_t bytes&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; g_bootloaderTree&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;read&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; dst&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; start&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; bytes&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;flexspi_nor_flash_clear_cache&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t instance&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 g_bootloaderTree&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;flexSpiNorDriver&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;clear_cache&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;


&lt;SPAN class="comment token"&gt;// Test data&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; flexspi_nor_config_t config&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; serial_nor_config_option_t option&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; status_t status&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; uint32_t instance &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Should identify NOR memory instance&lt;/SPAN&gt;

 



&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// Prepare Flash programming interface to internal Flash&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// WARNING: All access to the IAP flash routines must be with interrupts disabled&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// if code is executing from internal Flash&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// If HyperRAM is used in the system, this is NOT accessible at the same time as these&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// routines run, and you MUST re-initialize the HyperRAM interface after you are done &lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// using these IAP routines !&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;initIAP&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 option&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;option0&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;U &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xC0000008&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// QuadSPI NOR, Frequency: 133MHz&lt;/SPAN&gt;

 status &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;flexspi_nor_get_config&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;option&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; kStatus_Success&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  &lt;SPAN class="token function"&gt;messageDebug&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DBG_INFO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __MODULE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __LINE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"Error erasing, rc="&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

  &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

 status &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;flexspi_nor_flash_init&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; kStatus_Success&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  &lt;SPAN class="token function"&gt;messageDebug&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DBG_INFO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __MODULE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __LINE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"Error init, rc="&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; kStatus_Success&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;


&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// Erase an area in the internal 4 MByte Flash (granularity is 1 sector which is 4 KByte)&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// Flash is located at address 0x70000000 and is 0x400000 (4 MByte) in size&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// WARNING: All access to the IAP flash routines must be with interrupts disabled&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;eraseIAP&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; startaddress&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; length&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; address&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;for&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;address&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;startaddress &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x70000000&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; address&lt;SPAN class="operator token"&gt;&amp;lt;=&lt;/SPAN&gt;startaddress &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x70000000&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt; length&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; address&lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sectorSize&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  status &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;flexspi_nor_flash_erase&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; address &lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; config&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sectorSize&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Erase 1 sector&lt;/SPAN&gt;
  &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; kStatus_Success&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
   &lt;SPAN class="token function"&gt;messageDebug&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DBG_INFO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __MODULE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __LINE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"Error erasing, rc=%i, address=0x%08X"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x70000000&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt; address&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
   &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; kStatus_Success&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;


&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// Program an page (256 bytes) in the internal 4 MByte Flash&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// Flash is located at address 0x70000000 and is 0x400000 (4 MByte) in size&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;// WARNING: All access to the IAP flash routines must be with interrupts disabled&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;//------------------------------------------------------------------------------&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;programIAP&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; startAddress&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;page_buffer&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;// Program data to destination (256 bytes)&lt;/SPAN&gt;
 status &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;flexspi_nor_flash_page_program&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;instance&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;config&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; startAddress &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x70000000&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; page_buffer&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// program 1 page&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; kStatus_Success&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  &lt;SPAN class="token function"&gt;messageDebug&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DBG_INFO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __MODULE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; __LINE__&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"Error programming, rc=%i, address=0x%08X"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; startAddress&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; status&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; kStatus_Success&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;




‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And according to that, the driverstuff is located at&lt;/P&gt;&lt;P&gt;#define g_bootloaderTree (*(bootloader_api_entry_t**)(0x0020001c))&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And according to UM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/89855iDEB6F0656BB99E7D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:26:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948375#M4202</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2020-11-02T14:26:59Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948376#M4203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, according to the code you've provided, you really use the ROM API routines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, seems that the current version of the ROM NOR Flash API code really affects the FlexSPI1 controller when erase/program operations of the internal NOR Flash occur on FlexSPI2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I told before, I can raise a ticket to our R&amp;amp;D team to check the issue, but, anyway, there will be no fast solution for ROM code fix. The possible solution is to use non-ROM code running from some other place e.g. from RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 12:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948376#M4203</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-07-05T12:10:18Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948377#M4204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Arthur,&lt;/P&gt;&lt;P&gt;I tried getting the "flexspi_nor_flash_ops.c" functions to work, but no success (I gues LUT etc are not working for the internal Flash). Is there some samples for the internal NOR Flash using the SDK code ??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 13:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948377#M4204</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2019-07-05T13:15:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 programming the internal Flash at the same time as using HyperRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948378#M4205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SDK_x.y.z_EVK-MIMXRT1064\boards\evkmimxrt1064\driver_examples\flexspi\nor code seems to be the right one to try. Please try to bring it up using the MCUxpresso IDE. Also, please follow the SDK and IDE documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 09:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-programming-the-internal-Flash-at-the-same-time-as-using/m-p/948378#M4205</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-07-08T09:36:50Z</dc:date>
    </item>
  </channel>
</rss>