<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMXRT106x bootloader in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT106x-bootloader/m-p/947726#M4187</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sirs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read an paragraph in processor reference manual which says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"The ROM bootloader provides an API for the user application to boot from a new updated application safely after In-Application Programming (IAP) or re-enter serial downloader mode for image update. See more details in the next section."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, it is explained how to send ROM into boot mode using API: "runBootloader (&amp;amp;arg);"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One part of the "arg" is boot image selection (0, 1, 2 or 3). Can someone please explain to me what does this image selection refer to? Is there a way to store 4 different images to flash memory, and this is the way to tell ROM which one of them to boot after reset? If yes, where can I find information about this feature?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Than you,&lt;/P&gt;&lt;P&gt;Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Sep 2019 13:49:57 GMT</pubDate>
    <dc:creator>markomarusic25</dc:creator>
    <dc:date>2019-09-19T13:49:57Z</dc:date>
    <item>
      <title>IMXRT106x bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT106x-bootloader/m-p/947726#M4187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sirs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read an paragraph in processor reference manual which says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"The ROM bootloader provides an API for the user application to boot from a new updated application safely after In-Application Programming (IAP) or re-enter serial downloader mode for image update. See more details in the next section."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, it is explained how to send ROM into boot mode using API: "runBootloader (&amp;amp;arg);"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One part of the "arg" is boot image selection (0, 1, 2 or 3). Can someone please explain to me what does this image selection refer to? Is there a way to store 4 different images to flash memory, and this is the way to tell ROM which one of them to boot after reset? If yes, where can I find information about this feature?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Than you,&lt;/P&gt;&lt;P&gt;Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Sep 2019 13:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT106x-bootloader/m-p/947726#M4187</guid>
      <dc:creator>markomarusic25</dc:creator>
      <dc:date>2019-09-19T13:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT106x bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT106x-bootloader/m-p/947727#M4188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;One may refer to the thread&amp;nbsp;&lt;A href="https://community.nxp.com/message/1189574"&gt;https://community.nxp.com/message/1189574&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2019 02:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT106x-bootloader/m-p/947727#M4188</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2019-09-20T02:54:45Z</dc:date>
    </item>
  </channel>
</rss>