<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB high-speed regulator in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-high-speed-regulator/m-p/933381#M3841</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;Hi,&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;3V is generated from VBUS using LDO_USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;This 3V is for Full-Speed or Low-Speed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;These are described in 12.4.1.1.3 of the reference manual.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;However, high speed works at 400mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;Which regulator outputs 400mV?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;Is it possible to change this 400mV output?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="" title=""&gt;(Looking for the same function as the OUTPUT_TRG bit in the PMU_REG_3P0 register)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Yoshida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Oct 2019 06:43:27 GMT</pubDate>
    <dc:creator>yoshida_satoru</dc:creator>
    <dc:date>2019-10-01T06:43:27Z</dc:date>
    <item>
      <title>USB high-speed regulator</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-high-speed-regulator/m-p/933381#M3841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;Hi,&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;3V is generated from VBUS using LDO_USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;This 3V is for Full-Speed or Low-Speed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;These are described in 12.4.1.1.3 of the reference manual.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;However, high speed works at 400mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;Which regulator outputs 400mV?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;Is it possible to change this 400mV output?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="" title=""&gt;(Looking for the same function as the OUTPUT_TRG bit in the PMU_REG_3P0 register)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Yoshida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 06:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-high-speed-regulator/m-p/933381#M3841</guid>
      <dc:creator>yoshida_satoru</dc:creator>
      <dc:date>2019-10-01T06:43:27Z</dc:date>
    </item>
    <item>
      <title>Re: USB high-speed regulator</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-high-speed-regulator/m-p/933382#M3842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yoshida Satoru&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That 400 mV mentioned in the Reference Manual is only seen by the driver transceiver, so you actually will not have an output voltage for the High-speed transceiver regulator, you only have the Data lines working a the nominal 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this info helps&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 20:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-high-speed-regulator/m-p/933382#M3842</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-10-07T20:54:55Z</dc:date>
    </item>
  </channel>
</rss>