<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Profinet VS code example does not work on FRDM-IMXRT1186 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2408712#M37094</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263126"&gt;@ShellyZhang&lt;/a&gt;&amp;nbsp;Thanks very much!&lt;/P&gt;&lt;P&gt;The cyclic communication is&amp;nbsp;&lt;SPAN&gt;established if&amp;nbsp;GSDML-V2.45-portExample-test-20260120.xml&amp;nbsp; is applied. I choose the xml in the binary zip in previous operation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards!&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Aug 2026 07:46:39 GMT</pubDate>
    <dc:creator>wlfworld</dc:creator>
    <dc:date>2026-08-27T07:46:39Z</dc:date>
    <item>
      <title>Profinet VS code example does not work on FRDM-IMXRT1186</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2407665#M37072</link>
      <description>&lt;P&gt;I want to develop a PROFINET device based on RT11186 and test the profinet demo according to UG10320 V1.0, UG10455 V1.0 and AN15104 V1.0.&amp;nbsp; I did the following actions:&lt;/P&gt;&lt;P&gt;1. Extract the Profinet-Stack-Library and AN15104.zip.&lt;/P&gt;&lt;P&gt;2. Copy the frdm_pn.patch to the folder of Profinet stack and apply the patch according to the readme.&lt;/P&gt;&lt;P&gt;3. Manually change the project configuration according to prj.conf.rej/mcux_include.json.rej/mcuxpresso-tool.json.rej.&amp;nbsp; It is the same as the chapter 4.3 of AN15104.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The following definition has been included in the cakelist.txt.&amp;nbsp; They are not modified.&lt;/P&gt;&lt;P&gt;-DCPU_MIMXRT1186CVJ8C_cm33&lt;/P&gt;&lt;P&gt;-DMIMXRT1186_cm33_SERIES&lt;/P&gt;&lt;P&gt;-DXIP_BOOT_HEADER_ENABLE=1&lt;/P&gt;&lt;P&gt;4.&amp;nbsp; Add the "#if (defined(CPU_MIMXRT1186CVJ8C_cm7)... #ifndef configENABLE_FPU...." to enable FPU. This step is not included in the guide. Compiling will be failed if it is not modified, because the default CPU is RT1189 in FreeRTOSConfig.h.&amp;nbsp;&lt;/P&gt;&lt;P&gt;5. Import the Profinet project to VS code based on the SDK 2.6.3&lt;/P&gt;&lt;P&gt;6. Add the project "31_led_button" in the sysbuild.cmake according to step 8 and 9 of chapter 5 of UG10455.&lt;/P&gt;&lt;P&gt;7. Change the J12 and J18 of FRDM-IMXRT1186 to 1-2 connected to enable the NETC PHYs.&lt;/P&gt;&lt;P&gt;8. Build the project and download the image to&amp;nbsp;FRDM-IMXRT1186.&lt;/P&gt;&lt;P&gt;9. Install JDK, Npcap and Open the ICE. The ICE version is V1.7 and it is extraced from&amp;nbsp;port-ICE-202509180853-win32.win32.x86_64.zip.&lt;/P&gt;&lt;P&gt;10. The Profinet device is scaned sucessfully according to chapter 6 of UG10320.&lt;/P&gt;&lt;P&gt;11.&amp;nbsp; Set the DAP and module and Reduction Ratio according to Step1~7 of UG10320 chapter 7.1. It is failed when I click connect button according to step 8 of chapter 7.1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help me to analysis why it is failed to establish the cyclic communication?&lt;/P&gt;&lt;P&gt;Could you provide a profinet image of&amp;nbsp;FRDM-IMXRT1186 so I can check it is an issue of VS code project or IEC/hardware?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Aug 2026 05:34:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2407665#M37072</guid>
      <dc:creator>wlfworld</dc:creator>
      <dc:date>2026-08-24T05:34:38Z</dc:date>
    </item>
    <item>
      <title>Re: Profinet VS code example does not work on FRDM-IMXRT1186</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2407947#M37080</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265272"&gt;@wlfworld&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;I tested it on the RT1180 EVK and observed the same behavior: the device could be discovered during scanning, but the connection failed. Therefore, it does not appear to be related to your porting effort.&lt;/P&gt;
&lt;P&gt;We are currently investigating the issue internally. Once we identify the root cause or have any updates, we will get back to you as soon as possible.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Shelly&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 25 Aug 2026 03:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2407947#M37080</guid>
      <dc:creator>ShellyZhang</dc:creator>
      <dc:date>2026-08-25T03:31:12Z</dc:date>
    </item>
    <item>
      <title>Re: Profinet VS code example does not work on FRDM-IMXRT1186</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2408206#M37084</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265272"&gt;@wlfworld&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Which GSDML file did you use? I had previously used the wrong file, which is why I was unable to get it working. After switching to GSDML-V2.45-portExample-test-20260120.xml (located in Profinet-Stack-Library\RT1180_PROFINET_MCTC_LIB_GOAL_V_3_1_0-2\appl\goal_pnio\31_led_button), I was able to establish cyclic communication using the ICE tool.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ShellyZhang_0-1787654308913.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395303i98AE977BA9B21621/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ShellyZhang_0-1787654308913.png" alt="ShellyZhang_0-1787654308913.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Could you let me know at which step you are encountering the issue? If possible, could you share a screenshot? In general, if the PNIO device can be discovered during the scan, there is usually no major issue with the setup. You may also want to install Wireshark and check whether any PROFINET communication packets are being exchanged.&lt;/P&gt;
&lt;P&gt;If convenient, please upload your image file as well. I can test it on my side and compare the results.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Shelly&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 10:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2408206#M37084</guid>
      <dc:creator>ShellyZhang</dc:creator>
      <dc:date>2026-08-25T10:46:28Z</dc:date>
    </item>
    <item>
      <title>Re: Profinet VS code example does not work on FRDM-IMXRT1186</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2408712#M37094</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263126"&gt;@ShellyZhang&lt;/a&gt;&amp;nbsp;Thanks very much!&lt;/P&gt;&lt;P&gt;The cyclic communication is&amp;nbsp;&lt;SPAN&gt;established if&amp;nbsp;GSDML-V2.45-portExample-test-20260120.xml&amp;nbsp; is applied. I choose the xml in the binary zip in previous operation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Aug 2026 07:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2408712#M37094</guid>
      <dc:creator>wlfworld</dc:creator>
      <dc:date>2026-08-27T07:46:39Z</dc:date>
    </item>
    <item>
      <title>Re: Profinet VS code example does not work on FRDM-IMXRT1186</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2408727#M37095</link>
      <description>Hi wlfworld,&lt;BR /&gt;I'm very glad that you were able to resolve the issue. If you have any further questions, please feel free to create a new thread.&lt;BR /&gt;Best Regards,&lt;BR /&gt;Shelly</description>
      <pubDate>Thu, 27 Aug 2026 08:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Profinet-VS-code-example-does-not-work-on-FRDM-IMXRT1186/m-p/2408727#M37095</guid>
      <dc:creator>ShellyZhang</dc:creator>
      <dc:date>2026-08-27T08:24:31Z</dc:date>
    </item>
  </channel>
</rss>