<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RTC Power Calculation</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RTC-Power-Calculation/m-p/2401334#M36969</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260680"&gt;@specneeraj&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;VDD_SNVS_IN supplies power to the SNVS/RTC domain. This domain is an always-on, low-power domain that primarily maintains the 32 kHz RTC, SNVS logic, and related wake-up and safety functions. Its current consumption is only weakly correlated with the active/sleep states of CM7/CM4; therefore, the VDD_SNVS_IN values for the SNVS mode listed in Table 13 are not omitted “sleep-only” data, but rather baseline values that can be used in RTC backup scenarios.&lt;/P&gt;
&lt;DIV&gt;
&lt;UL&gt;
&lt;LI&gt;If the coin cell only provides power when the main power source fails → Use the SNVS mode current estimate directly;&lt;/LI&gt;
&lt;LI&gt;If the coin cell also supplies power to &lt;CODE&gt;VDD_SNVS_IN&lt;/CODE&gt; while the system is active, calculate the average current based on the active/SNVS duty cycle.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The main factors affecting the SNVS current include temperature,&amp;nbsp;&lt;CODE class=""&gt;VDD_SNVS_IN&lt;/CODE&gt;&amp;nbsp;voltage, process variations, leakage from the 32 kHz RTC crystal/board, external leakage from SNVS-related pins, and whether the device has actually entered SNVS mode. Please refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN13104.pdf" target="_blank"&gt;AN13104&lt;/A&gt; for more details.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;/DIV&gt;
&lt;DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;/DIV&gt;</description>
    <pubDate>Mon, 03 Aug 2026 07:15:33 GMT</pubDate>
    <dc:creator>Gavin_Jia</dc:creator>
    <dc:date>2026-08-03T07:15:33Z</dc:date>
    <item>
      <title>RTC Power Calculation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RTC-Power-Calculation/m-p/2400327#M36956</link>
      <description>&lt;P&gt;Hello NXP,&lt;BR /&gt;&lt;BR /&gt;We are calculating battery life for RTC for which active &amp;amp; sleep current are required for SNVS power domain in RT1176.&lt;/P&gt;&lt;P&gt;However refer to datsheet IMXRT1170BIEC - Table13, page 35, only sleep current is given.&lt;/P&gt;&lt;P&gt;Please let us know the factors affecting the active current and various calculations related to active current for the SNVS power domain.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jul 2026 04:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RTC-Power-Calculation/m-p/2400327#M36956</guid>
      <dc:creator>specneeraj</dc:creator>
      <dc:date>2026-07-30T04:54:49Z</dc:date>
    </item>
    <item>
      <title>Re: RTC Power Calculation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RTC-Power-Calculation/m-p/2401334#M36969</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260680"&gt;@specneeraj&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;VDD_SNVS_IN supplies power to the SNVS/RTC domain. This domain is an always-on, low-power domain that primarily maintains the 32 kHz RTC, SNVS logic, and related wake-up and safety functions. Its current consumption is only weakly correlated with the active/sleep states of CM7/CM4; therefore, the VDD_SNVS_IN values for the SNVS mode listed in Table 13 are not omitted “sleep-only” data, but rather baseline values that can be used in RTC backup scenarios.&lt;/P&gt;
&lt;DIV&gt;
&lt;UL&gt;
&lt;LI&gt;If the coin cell only provides power when the main power source fails → Use the SNVS mode current estimate directly;&lt;/LI&gt;
&lt;LI&gt;If the coin cell also supplies power to &lt;CODE&gt;VDD_SNVS_IN&lt;/CODE&gt; while the system is active, calculate the average current based on the active/SNVS duty cycle.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The main factors affecting the SNVS current include temperature,&amp;nbsp;&lt;CODE class=""&gt;VDD_SNVS_IN&lt;/CODE&gt;&amp;nbsp;voltage, process variations, leakage from the 32 kHz RTC crystal/board, external leakage from SNVS-related pins, and whether the device has actually entered SNVS mode. Please refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN13104.pdf" target="_blank"&gt;AN13104&lt;/A&gt; for more details.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;/DIV&gt;
&lt;DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Mon, 03 Aug 2026 07:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RTC-Power-Calculation/m-p/2401334#M36969</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2026-08-03T07:15:33Z</dc:date>
    </item>
  </channel>
</rss>