<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Create a second stage HAB authenticated application image (bootloader + app)</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Create-a-second-stage-HAB-authenticated-application-image/m-p/2362226#M36570</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243200"&gt;@rd24&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We provide an example for your case, please kindly refer to&amp;nbsp;&lt;A href="https://github.com/nxp-mcuxpresso/mcuxsdk-examples/tree/release/25.12.00/ota_examples/mcuboot_opensource" target="_blank"&gt;https://github.com/nxp-mcuxpresso/mcuxsdk-examples/tree/release/25.12.00/ota_examples/mcuboot_opensource&lt;/A&gt;&amp;nbsp;for details. The tools mentioned are tested with mcuboot so far, we haven't checked with any custom bootloader , so maybe you need some adaption here. To create a bootable app image by a secondary boot loader, you have to remove its IVT header as well as adjusting the starting address. Did you do these on&amp;nbsp;&lt;SPAN&gt;the blinky example from the RT1040 SDK? Please kindly clarify.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 08 May 2026 03:33:07 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2026-05-08T03:33:07Z</dc:date>
    <item>
      <title>Create a second stage HAB authenticated application image (bootloader + app)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Create-a-second-stage-HAB-authenticated-application-image/m-p/2360076#M36552</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to create a two stage secure boot work flow on i.MXRT1040. I have a custom bootloader and an application. I want the ROM code HAB to authenticate the bootloader and the bootloader to use HAB API to authenticate the application.&lt;/P&gt;&lt;P&gt;I am using MCUXpresso Secure Provisioning Tool v25.12 for signing the images. Both bootloader and application images are&amp;nbsp;XIP Flash images.&lt;/P&gt;&lt;P&gt;Below is my Flash layout:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Custom bootloader at address 0x60000000, authenticated by ROM HAB Code&lt;/LI&gt;&lt;LI&gt;Application at address 0x600C0000, to be authenticated by bootloader using HAB API&lt;/LI&gt;&lt;/UL&gt;&lt;LI-CODE lang="c"&gt;  /* Bootloader flash memory */
  m_flash_cfg_bl        (RX)  : ORIGIN = 0x60000000, LENGTH = 0x00001000
  m_ivt_bl              (RX)  : ORIGIN = 0x60001000, LENGTH = 0x00001000
  m_intrs_flash_bl      (RX)  : ORIGIN = 0x60002000, LENGTH = 0x00000400
  m_text_bl             (RX)  : ORIGIN = 0x60002400, LENGTH = 0x0007DC00

  /* Application flash memory */
  m_flash_cfg_app       (RX)  : ORIGIN = 0x600C0000, LENGTH = 0x00001000
  m_ivt_app             (RX)  : ORIGIN = 0x600C1000, LENGTH = 0x00001000
  m_intrs_flash_app     (RX)  : ORIGIN = 0x600C2000, LENGTH = 0x00000400
  m_text_app            (RX)  : ORIGIN = 0x600C2400, LENGTH = 0x000FDBA0&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have achieved the 1st stage where the ROM code authenticates the bootloader and I don't get any HAB events.&lt;/P&gt;&lt;P&gt;For the application, I am currently using the blinky example from the RT1040 SDK and compiled bin file is about 13 KB. When I sign this bin using the SEC GUI tool, the signed binary becomes 788 KB. I am using start address parameter as 0x600C0000. This is not the case for the bootloader signed bin as the start address is 0x60000000.&lt;/P&gt;&lt;P&gt;I inspected the application's bin file and found at offset 0 the Image Vector Table (IVT) exists and the program code starts offset 0x000BF000, in between everything is zeros. I expect the program code to start 0x1000 bytes after the IVT as per the linker script provided above (which is the case for the bootloader signed bin). If I flash this application binary at Flash location 0x600C0000, then my bootloader will not be able to start the application as there will be zeros at the jump address.&lt;/P&gt;&lt;P&gt;So, my questions are:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is this bootloader + app HAB workflow possible and supported by the SEC tool?&lt;/LI&gt;&lt;LI&gt;If yes, how can I create the correct signed binary for my application using this tool?&lt;/LI&gt;&lt;LI&gt;Are there any other tools I should use for this scenario?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 04 May 2026 12:47:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Create-a-second-stage-HAB-authenticated-application-image/m-p/2360076#M36552</guid>
      <dc:creator>rd24</dc:creator>
      <dc:date>2026-05-04T12:47:02Z</dc:date>
    </item>
    <item>
      <title>Re: Create a second stage HAB authenticated application image (bootloader + app)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Create-a-second-stage-HAB-authenticated-application-image/m-p/2362226#M36570</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243200"&gt;@rd24&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We provide an example for your case, please kindly refer to&amp;nbsp;&lt;A href="https://github.com/nxp-mcuxpresso/mcuxsdk-examples/tree/release/25.12.00/ota_examples/mcuboot_opensource" target="_blank"&gt;https://github.com/nxp-mcuxpresso/mcuxsdk-examples/tree/release/25.12.00/ota_examples/mcuboot_opensource&lt;/A&gt;&amp;nbsp;for details. The tools mentioned are tested with mcuboot so far, we haven't checked with any custom bootloader , so maybe you need some adaption here. To create a bootable app image by a secondary boot loader, you have to remove its IVT header as well as adjusting the starting address. Did you do these on&amp;nbsp;&lt;SPAN&gt;the blinky example from the RT1040 SDK? Please kindly clarify.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 08 May 2026 03:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Create-a-second-stage-HAB-authenticated-application-image/m-p/2362226#M36570</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2026-05-08T03:33:07Z</dc:date>
    </item>
    <item>
      <title>Re: Create a second stage HAB authenticated application image (bootloader + app)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Create-a-second-stage-HAB-authenticated-application-image/m-p/2372393#M36653</link>
      <description>&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;Sorry for the late reply.&lt;/P&gt;&lt;P&gt;I did some changes and now am able to build a smaller image with correct offset. Here is what I did:&lt;/P&gt;&lt;P&gt;1. First I generate the build script with this command:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;securep -w /wksp/rt1040SecAppWksp1/ --device MIMXRT1040 --boot-device Winbond_W25Q64JW --boot-type authenticated_hab --life-cycle open_develop --script-only build --source-image iled_blinky.bin --start-address 0x600c1000 --img-cert crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem --save-settings&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Then I modified the following configurations in `configs/imx_application_gen.yaml`&lt;/P&gt;&lt;LI-CODE lang="c"&gt;startAddress: 0x600c0000
ivtOffset: 0x0
initialLoadSize: 0x1000&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. Then I call the script `./build_image_lnx.sh` to build the signed image.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I am trying to authenticate the blinky signed binary from my bootloader, but getting HAB authentication failure when my bootloader is calling `hab_rvt::authenticate_image_no_dcd`. The audit log I get from the `hab_rvt::report_event` says &lt;SPAN&gt;HAB_INV_ADDRESS&lt;/SPAN&gt;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;DB 00 08 43 33 22 0A 00                           |  ...C3"..&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the linker I modified for the blinky example:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;MEMORY
{
  m_ivt                 (RX)  : ORIGIN = 0x600C0000, LENGTH = 0x00001000
  m_interrupts          (RX)  : ORIGIN = 0x600C1000, LENGTH = 0x00000400
  m_text                (RX)  : ORIGIN = 0x600C1400, LENGTH = 0x007FDC00
  m_qacode              (RX)  : ORIGIN = 0x00000000, LENGTH = 0x00020000
  m_data                (RW)  : ORIGIN = 0x20000000, LENGTH = 0x00020000
  m_data2               (RW)  : ORIGIN = 0x20200000, LENGTH = 0x00040000
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for your questions, I adjusted the startAddress to 0x600c0000. Could you please explain what you mean by "&lt;SPAN&gt;you have to remove its IVT header&lt;/SPAN&gt;"? Please note the bootloader I am using to verify the blinky signed binary is not signed as of now.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rohan&lt;/P&gt;</description>
      <pubDate>Thu, 28 May 2026 09:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Create-a-second-stage-HAB-authenticated-application-image/m-p/2372393#M36653</guid>
      <dc:creator>rd24</dc:creator>
      <dc:date>2026-05-28T09:53:09Z</dc:date>
    </item>
  </channel>
</rss>