<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: AN14808, can not find some functions in the document in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2354525#M36518</link>
    <description>&lt;P&gt;I have found it in AN14808SW.zip, but in the document chapter 3.7, item b., it seems miss something in&amp;nbsp;&lt;/P&gt;&lt;P&gt;case USB_HostCdcEcmRunDial:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 22 Apr 2026 06:06:03 GMT</pubDate>
    <dc:creator>felix1</dc:creator>
    <dc:date>2026-04-22T06:06:03Z</dc:date>
    <item>
      <title>AN14808, can not find some functions in the document</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2354478#M36516</link>
      <description>&lt;P&gt;In the AN14808, connect i.MX RT1170 to Quectel EC200A-CN USB 4G modem,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/AN14808/page/topics/details_for_implementation.html" target="_blank"&gt;https://docs.nxp.com/bundle/AN14808/page/topics/details_for_implementation.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;can not find some functions in the document chapter 3.7, item g.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;USB_HostCdcECM_ATInCallback();
USB_HostCdcECM_ATOutCallback();
dial_update_status();
dial_tx();
dial_rx();
lte_dial();
USB_HostCdcECM_EC200A_EP0_Callback();
update_ec200a_status();
ep0_communicate();
init_ec200a();                 &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;Where can find these sample code functions?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Apr 2026 03:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2354478#M36516</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2026-04-22T03:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: AN14808, can not find some functions in the document</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2354525#M36518</link>
      <description>&lt;P&gt;I have found it in AN14808SW.zip, but in the document chapter 3.7, item b., it seems miss something in&amp;nbsp;&lt;/P&gt;&lt;P&gt;case USB_HostCdcEcmRunDial:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Apr 2026 06:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2354525#M36518</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2026-04-22T06:06:03Z</dc:date>
    </item>
    <item>
      <title>Re: AN14808, can not find some functions in the document</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2356010#M36535</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160932"&gt;@felix1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In this case, you would need to add the missing part of:&lt;/P&gt;
&lt;PRE&gt;&lt;SPAN&gt;case USB_HostCdcEcmRunDial&lt;/SPAN&gt;&lt;/PRE&gt;
&lt;P&gt;In order for it to match what you see on section d) of "7. In usb_ethernetif_freertos.c:"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Apr 2026 20:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2356010#M36535</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2026-04-24T20:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: AN14808, can not find some functions in the document</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2356527#M36537</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I don't have RT1170 EVK and Quectel EC200A-CN, I use RT1020 EVK and EC200U-EU&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;C4-P01 EVB&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://developer.quectel.com/doc/quecpython/Dev_board_guide/en/ec200x-evb.html" target="_blank" rel="noopener"&gt;https://developer.quectel.com/doc/quecpython/Dev_board_guide/en/ec200x-evb.html&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;to test this application note.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For now, can not trigger the EC200U-EU EVB USB device attached, just show the log&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;USB host init success.&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;I check the host&amp;nbsp;CONTROLLER_ID, and it seems correct for RT1020.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;#if ((defined USB_HOST_CONFIG_EHCI) &amp;amp;&amp;amp; (USB_HOST_CONFIG_EHCI))
#ifndef CONTROLLER_ID
#define CONTROLLER_ID kUSB_ControllerEhci0
#endif
#endif /* USB_HOST_CONFIG_EHCI */&lt;/LI-CODE&gt;&lt;P&gt;Is there any USB difference I need to modify?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Apr 2026 10:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2356527#M36537</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2026-04-27T10:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: AN14808, can not find some functions in the document</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2359888#M36550</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Anyone have tested the application note before? Can you give your hardware environment for reference, like RTXXXX EVK, Quectel modem module.&lt;/P&gt;</description>
      <pubDate>Mon, 04 May 2026 03:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2359888#M36550</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2026-05-04T03:09:20Z</dc:date>
    </item>
    <item>
      <title>Re: AN14808, can not find some functions in the document</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2362599#M36572</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160932"&gt;@felix1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Considering that the AppNote was used for the RT1170 and that you are currently using an RT1020, I would highly suggest you check the USB example codes we provide on the RT1020 SDK as reference to ensure that the USB peripheral on the RT1020 is properly initialized according to its clock tree, power controls, and specific PHY requirements.&lt;/P&gt;</description>
      <pubDate>Fri, 08 May 2026 22:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AN14808-can-not-find-some-functions-in-the-document/m-p/2362599#M36572</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2026-05-08T22:03:33Z</dc:date>
    </item>
  </channel>
</rss>