<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1176 Custom Board Bring-up: Boot from SPI NAND (W25N512G) and Initial Firmware Download Issue in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-Custom-Board-Bring-up-Boot-from-SPI-NAND-W25N512G-and/m-p/2343987#M36445</link>
    <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a custom board based on the MIMXRT1176CVM8A MCU and currently in the board bring-up phase.&lt;/P&gt;&lt;P&gt;For reference, I am using the RT1176 EVKB, which uses W25Q512 QSPI NOR Flash for booting. However, in our custom board design, we have used W25N512G SPI NAND Flash instead of QSPI NOR Flash.&lt;/P&gt;&lt;P&gt;Currently, I am facing issues with downloading and running firmware on the custom board.&lt;/P&gt;&lt;P&gt;I would like to clarify the following:&lt;/P&gt;&lt;P&gt;Does RT1176 support booting directly from SPI NAND Flash (W25N512G)?&lt;BR /&gt;If SPI NAND boot is not supported, what is the recommended boot source for custom boards?&lt;BR /&gt;In the absence of QSPI NOR Flash, what is the correct method to download firmware for the first time?&lt;BR /&gt;Can Serial Downloader mode (USB/UART) be used reliably in this case?&lt;BR /&gt;Are there any reference examples or application notes for using SPI NAND Flash with RT1176 for storage purposes?&lt;/P&gt;&lt;P&gt;Additional information:&lt;/P&gt;&lt;P&gt;SDRAM is used in the design and configured similar to EVKB.&lt;BR /&gt;Facing issues during debug and flashing (core not detected / unable to run code).&lt;/P&gt;&lt;P&gt;Any suggestions or guidance would be very helpful.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256480"&gt;@meetbhatt2113&lt;/a&gt;&amp;nbsp;&lt;/DIV&gt;&lt;SPAN class=""&gt;Select to translate &lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;@rt1176evk&lt;/P&gt;</description>
    <pubDate>Thu, 02 Apr 2026 05:21:27 GMT</pubDate>
    <dc:creator>RAVIRAJ123</dc:creator>
    <dc:date>2026-04-02T05:21:27Z</dc:date>
    <item>
      <title>RT1176 Custom Board Bring-up: Boot from SPI NAND (W25N512G) and Initial Firmware Download Issue</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-Custom-Board-Bring-up-Boot-from-SPI-NAND-W25N512G-and/m-p/2343987#M36445</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a custom board based on the MIMXRT1176CVM8A MCU and currently in the board bring-up phase.&lt;/P&gt;&lt;P&gt;For reference, I am using the RT1176 EVKB, which uses W25Q512 QSPI NOR Flash for booting. However, in our custom board design, we have used W25N512G SPI NAND Flash instead of QSPI NOR Flash.&lt;/P&gt;&lt;P&gt;Currently, I am facing issues with downloading and running firmware on the custom board.&lt;/P&gt;&lt;P&gt;I would like to clarify the following:&lt;/P&gt;&lt;P&gt;Does RT1176 support booting directly from SPI NAND Flash (W25N512G)?&lt;BR /&gt;If SPI NAND boot is not supported, what is the recommended boot source for custom boards?&lt;BR /&gt;In the absence of QSPI NOR Flash, what is the correct method to download firmware for the first time?&lt;BR /&gt;Can Serial Downloader mode (USB/UART) be used reliably in this case?&lt;BR /&gt;Are there any reference examples or application notes for using SPI NAND Flash with RT1176 for storage purposes?&lt;/P&gt;&lt;P&gt;Additional information:&lt;/P&gt;&lt;P&gt;SDRAM is used in the design and configured similar to EVKB.&lt;BR /&gt;Facing issues during debug and flashing (core not detected / unable to run code).&lt;/P&gt;&lt;P&gt;Any suggestions or guidance would be very helpful.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256480"&gt;@meetbhatt2113&lt;/a&gt;&amp;nbsp;&lt;/DIV&gt;&lt;SPAN class=""&gt;Select to translate &lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;@rt1176evk&lt;/P&gt;</description>
      <pubDate>Thu, 02 Apr 2026 05:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-Custom-Board-Bring-up-Boot-from-SPI-NAND-W25N512G-and/m-p/2343987#M36445</guid>
      <dc:creator>RAVIRAJ123</dc:creator>
      <dc:date>2026-04-02T05:21:27Z</dc:date>
    </item>
  </channel>
</rss>