<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Secure Boot in IMXRT1170 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/2343887#M36443</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Where can I find AN13250?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Apr 2026 01:22:09 GMT</pubDate>
    <dc:creator>mnh-2014</dc:creator>
    <dc:date>2026-04-02T01:22:09Z</dc:date>
    <item>
      <title>Secure Boot in IMXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1491859#M20695</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We want to use secure boot HAB functionality on IMXRT1170 Eval-Kit.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. Can you tell us is there a sample code for testing secure boot functionality? if yes, Can we modify the bootloader code what are the steps for it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Is secure boot (HAB)functionality support on RTOS MQX V5 on IMX RT 1170?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;3. What tools I need to use for this secure bootloader application?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 14:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1491859#M20695</guid>
      <dc:creator>Naveed</dc:creator>
      <dc:date>2022-07-19T14:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot in IMXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1493545#M20746</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;1. Please refer to AN13250. This AN describes how to enable the secure boots in RT1170 additionally, it refers to multiple documents that can be helpful.&lt;BR /&gt;2. The HAB is the mechanism that assures that only authorized images execute in our device, so if the MQX application is signed correctly, the device should execute it correctly.&lt;BR /&gt;3. You can use Secure Provisioning Tool: &lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;MCUBootUtility can also be used to sign images to be executed by HAB: &lt;A href="https://github.com/JayHeng/NXP-MCUBootUtility" target="_blank"&gt;https://github.com/JayHeng/NXP-MCUBootUtility&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Additionally, this post might be helpful: &lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1050-HAB-Encrypted-Image-Generation-and-Analysis/ta-p/1124877" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1050-HAB-Encrypted-Image-Generation-and-Analysis/ta-p/1124877&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 18:39:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1493545#M20746</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-07-21T18:39:50Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot in IMXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1709150#M26534</link>
      <description>&lt;P&gt;Is the same applicable for RT1060?&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 13:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1709150#M26534</guid>
      <dc:creator>pm_2552</dc:creator>
      <dc:date>2023-08-22T13:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot in IMXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1893339#M30989</link>
      <description>&lt;P&gt;Cannot find AN&lt;SPAN&gt;13250. Is it moved to some other location or under some other application note?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 05:58:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/1893339#M30989</guid>
      <dc:creator>Gaurav13</dc:creator>
      <dc:date>2024-06-25T05:58:41Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot in IMXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/2343887#M36443</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Where can I find AN13250?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Apr 2026 01:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-in-IMXRT1170/m-p/2343887#M36443</guid>
      <dc:creator>mnh-2014</dc:creator>
      <dc:date>2026-04-02T01:22:09Z</dc:date>
    </item>
  </channel>
</rss>