<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Hardware Design Guide for MIMXRT1062DVN6B (NVCC_SPIX) in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Hardware-Design-Guide-for-MIMXRT1062DVN6B-NVCC-SPIX/m-p/2343373#M36434</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/87774"&gt;@bennxp&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;The official documentation does not provide a hardware development manual specific to the RT1060X. Regarding NVCC_SPIX, these are new, independent power domains that support either 1.8V or 3.3V. For the selection of decoupling capacitors, refer to NVCC_GPIO; please do not skimp on capacitors. There are no special requirements regarding power-up sequencing.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2026-04-01_11-43-50.png" style="width: 481px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/380997iA5D3C51AD01955A9/image-size/large?v=v2&amp;amp;px=999" role="button" title="2026-04-01_11-43-50.png" alt="2026-04-01_11-43-50.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Apr 2026 03:45:09 GMT</pubDate>
    <dc:creator>Gavin_Jia</dc:creator>
    <dc:date>2026-04-01T03:45:09Z</dc:date>
    <item>
      <title>Hardware Design Guide for MIMXRT1062DVN6B (NVCC_SPIX)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Hardware-Design-Guide-for-MIMXRT1062DVN6B-NVCC-SPIX/m-p/2343242#M36432</link>
      <description>&lt;P&gt;Is there a hardware design guide for the&amp;nbsp;MIMXRT1062DVN6B? (ie the 1060X series)? The latest I see is&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/MIMXRT105060HDUG/page/topics/power_supply.html" target="_self"&gt;MIMXRT105060HDUG&lt;/A&gt;&amp;nbsp;which doesn't mention the extra SPI0 and SPI1 banks in the 225-pin package. I'm looking to confirm if the NVCC_SPI0 and NVCC_SPI1 can be powered with 1.8Vor 3.3V like the NCC_SD0 / NVCC_SD1 banks. Also any information about recommended number / value of decoupling caps for those banks and power sequencing would be great as well.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Tue, 31 Mar 2026 20:32:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Hardware-Design-Guide-for-MIMXRT1062DVN6B-NVCC-SPIX/m-p/2343242#M36432</guid>
      <dc:creator>bennxp</dc:creator>
      <dc:date>2026-03-31T20:32:10Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware Design Guide for MIMXRT1062DVN6B (NVCC_SPIX)</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Hardware-Design-Guide-for-MIMXRT1062DVN6B-NVCC-SPIX/m-p/2343373#M36434</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/87774"&gt;@bennxp&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;The official documentation does not provide a hardware development manual specific to the RT1060X. Regarding NVCC_SPIX, these are new, independent power domains that support either 1.8V or 3.3V. For the selection of decoupling capacitors, refer to NVCC_GPIO; please do not skimp on capacitors. There are no special requirements regarding power-up sequencing.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2026-04-01_11-43-50.png" style="width: 481px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/380997iA5D3C51AD01955A9/image-size/large?v=v2&amp;amp;px=999" role="button" title="2026-04-01_11-43-50.png" alt="2026-04-01_11-43-50.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Apr 2026 03:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Hardware-Design-Guide-for-MIMXRT1062DVN6B-NVCC-SPIX/m-p/2343373#M36434</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2026-04-01T03:45:09Z</dc:date>
    </item>
  </channel>
</rss>