<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Evaluation board for high channel count UAC2 on RT1176 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Evaluation-board-for-high-channel-count-UAC2-on-RT1176/m-p/2342557#M36427</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182695"&gt;@simmania&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;RT1170 Version B is primarily intended to fix&amp;nbsp;ERR052351 and&amp;nbsp;ERR050643.&amp;nbsp;&lt;BR /&gt;You can find more details in this AN:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14716.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN14716.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The RT1170-EVKB is suitable for your application scenario.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
    <pubDate>Tue, 31 Mar 2026 06:33:35 GMT</pubDate>
    <dc:creator>Gavin_Jia</dc:creator>
    <dc:date>2026-03-31T06:33:35Z</dc:date>
    <item>
      <title>Evaluation board for high channel count UAC2 on RT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Evaluation-board-for-high-channel-count-UAC2-on-RT1176/m-p/2342308#M36426</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I want to create an audio product that needs to input a large number of audio channels through USB. So I want to use UAC2 for this.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I noticed that the USB controller had some isochronous problems in early RT silicon. For this reason there seems to be a "RT1060-with USB Fix" version of the RT1060. I did not see such a version of the RT1176. Though there is a RT1176-B silicon version with less USB bugs. So I guess I should use this B-version.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But there is no evaluation board using the B-silicon. Even the&amp;nbsp;&lt;SPAN class=""&gt;MIMXRT1170-EVKB uses A-silicon version (&lt;SPAN&gt;MIMXRT1176DVMAA&lt;/SPAN&gt;&amp;nbsp;in stead of &lt;SPAN&gt;MIMXRT1176DVMAB&lt;/SPAN&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;So how can I start to develop this? Is there a suitable evaluation kit?&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Mar 2026 16:13:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Evaluation-board-for-high-channel-count-UAC2-on-RT1176/m-p/2342308#M36426</guid>
      <dc:creator>simmania</dc:creator>
      <dc:date>2026-03-30T16:13:40Z</dc:date>
    </item>
    <item>
      <title>Re: Evaluation board for high channel count UAC2 on RT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Evaluation-board-for-high-channel-count-UAC2-on-RT1176/m-p/2342557#M36427</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182695"&gt;@simmania&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;RT1170 Version B is primarily intended to fix&amp;nbsp;ERR052351 and&amp;nbsp;ERR050643.&amp;nbsp;&lt;BR /&gt;You can find more details in this AN:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14716.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN14716.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The RT1170-EVKB is suitable for your application scenario.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Tue, 31 Mar 2026 06:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Evaluation-board-for-high-channel-count-UAC2-on-RT1176/m-p/2342557#M36427</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2026-03-31T06:33:35Z</dc:date>
    </item>
    <item>
      <title>Re: Evaluation board for high channel count UAC2 on RT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Evaluation-board-for-high-channel-count-UAC2-on-RT1176/m-p/2342866#M36429</link>
      <description>&lt;P&gt;And which silicon versions are suitable for our application? We may prefer a smaller RT device like RT1060.&lt;BR /&gt;For the RT1060 I assume we need the B-version because of the USB-Bug-fix.&lt;BR /&gt;But as far as I know the RT1010, RT1020, RT1040 and RT1050 series do not have B-version silicon. Do they have the same core as the RT1060, and thus the same USB bug for isochronous transfers?&lt;/P&gt;</description>
      <pubDate>Tue, 31 Mar 2026 10:21:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Evaluation-board-for-high-channel-count-UAC2-on-RT1176/m-p/2342866#M36429</guid>
      <dc:creator>simmania</dc:creator>
      <dc:date>2026-03-31T10:21:05Z</dc:date>
    </item>
  </channel>
</rss>