<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMX RT1176-EVKB Genavb/TSN synchronization failed. in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMX-RT1176-EVKB-Genavb-TSN-synchronization-failed/m-p/2339099#M36405</link>
    <description>&lt;P&gt;When I was testing GPTP using two MIMXRT1176-EVKB boards, I found that the two development boards could not synchronize successfully. I needed to add compensation to the ports, but after compensation, the synchronization was successful. I was able to distinguish between master and slave. Then, I tested the AS accuracy through the PPS signal and found that the error was about 18us. What debugging methods can I use to reduce the link latency?&lt;/P&gt;</description>
    <pubDate>Wed, 25 Mar 2026 09:14:06 GMT</pubDate>
    <dc:creator>ZhaoXingLi</dc:creator>
    <dc:date>2026-03-25T09:14:06Z</dc:date>
    <item>
      <title>MIMX RT1176-EVKB Genavb/TSN synchronization failed.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMX-RT1176-EVKB-Genavb-TSN-synchronization-failed/m-p/2339099#M36405</link>
      <description>&lt;P&gt;When I was testing GPTP using two MIMXRT1176-EVKB boards, I found that the two development boards could not synchronize successfully. I needed to add compensation to the ports, but after compensation, the synchronization was successful. I was able to distinguish between master and slave. Then, I tested the AS accuracy through the PPS signal and found that the error was about 18us. What debugging methods can I use to reduce the link latency?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Mar 2026 09:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMX-RT1176-EVKB-Genavb-TSN-synchronization-failed/m-p/2339099#M36405</guid>
      <dc:creator>ZhaoXingLi</dc:creator>
      <dc:date>2026-03-25T09:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX RT1176-EVKB Genavb/TSN synchronization failed.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMX-RT1176-EVKB-Genavb-TSN-synchronization-failed/m-p/2339817#M36411</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261007"&gt;@ZhaoXingLi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;I'm not entirely sure how you arrived at the compensation value of -36.5 us, but it seems a bit too high. Have you tried setting both &lt;SPAN data-teams="true"&gt;rxDelayCompensation and txDelayCompensation at the same time?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;Also, the final 18us error is unusual. Could there be an issue with the connection? Why not try using a different Ethernet cable to check? Thanks!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;Best regards,&lt;BR /&gt;Gavin&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Mar 2026 07:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMX-RT1176-EVKB-Genavb-TSN-synchronization-failed/m-p/2339817#M36411</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2026-03-26T07:16:15Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX RT1176-EVKB Genavb/TSN synchronization failed.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMX-RT1176-EVKB-Genavb-TSN-synchronization-failed/m-p/2339872#M36414</link>
      <description>&lt;P&gt;Hi@&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203261" target="_blank" rel="noopener"&gt;&lt;SPAN class=""&gt;Gavin_Jia&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;thank you for your reply. I apologize, it was my mistake. The 18µs error was because I didn't perform port compensation on the development board and the GPTP synchronization failed during testing. After compensating for txDelayCompensation and rxDelayCompensation, the AS accuracy tested via PPS was around 20ns. I would like to ask if this error range is normal? Also, without port compensation and setting GPTP synchronization to fail, I can't distinguish between master and slave. Are there any other solutions for this? Looking forward to your reply, thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Mar 2026 08:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMX-RT1176-EVKB-Genavb-TSN-synchronization-failed/m-p/2339872#M36414</guid>
      <dc:creator>ZhaoXingLi</dc:creator>
      <dc:date>2026-03-26T08:23:16Z</dc:date>
    </item>
  </channel>
</rss>