<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT1020-EVK FlexCAN pin mapping and CAN hardware availability in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1020-EVK-FlexCAN-pin-mapping-and-CAN-hardware-availability/m-p/2322821#M36250</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260217"&gt;@Tasnim&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;The schematic for the RT1020-EVK is available on this&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MIMXRT1020-EVK" target="_self"&gt; web page&lt;/A&gt;. The EVK board includes the TJA1057GT/3.&lt;/P&gt;
&lt;P&gt;Details regarding the question can be found on Page 7 of this schematic.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;DIV id="tinyMceEditorGavin_Jia_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 26 Feb 2026 02:38:41 GMT</pubDate>
    <dc:creator>Gavin_Jia</dc:creator>
    <dc:date>2026-02-26T02:38:41Z</dc:date>
    <item>
      <title>MIMXRT1020-EVK FlexCAN pin mapping and CAN hardware availability</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1020-EVK-FlexCAN-pin-mapping-and-CAN-hardware-availability/m-p/2322769#M36249</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the MIMXRT1020-EVK board and trying to use FlexCAN.&lt;/P&gt;&lt;P&gt;From the i.MXRT1020 reference manual, I see that FLEXCAN1 can be mapped to multiple pins, for example:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;FLEXCAN1_TX → GPIO_AD_B0_04 (ALT1)&lt;/LI&gt;&lt;LI&gt;FLEXCAN1_RX → GPIO_AD_B0_05 (ALT1)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, on the MIMXRT1020-EVK board:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I cannot find any onboard CAN transceiver (e.g., TJA1057)&lt;/LI&gt;&lt;LI&gt;I do not see any CAN connector (CANH/CANL)&lt;/LI&gt;&lt;LI&gt;The Arduino headers are unpopulated, so it is unclear which pins are actually routed&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Could you please clarify:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Which exact pins are used for FLEXCAN1 on the MIMXRT1020-EVK?&lt;/LI&gt;&lt;LI&gt;Are GPIO_AD_B0_04 and GPIO_AD_B0_05 routed to any accessible header?&lt;/LI&gt;&lt;LI&gt;Is there any onboard CAN transceiver or should an external transceiver be used?&lt;/LI&gt;&lt;LI&gt;If possible, which header pins correspond to these signals?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Feb 2026 00:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1020-EVK-FlexCAN-pin-mapping-and-CAN-hardware-availability/m-p/2322769#M36249</guid>
      <dc:creator>Tasnim</dc:creator>
      <dc:date>2026-02-26T00:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1020-EVK FlexCAN pin mapping and CAN hardware availability</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1020-EVK-FlexCAN-pin-mapping-and-CAN-hardware-availability/m-p/2322821#M36250</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260217"&gt;@Tasnim&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;The schematic for the RT1020-EVK is available on this&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MIMXRT1020-EVK" target="_self"&gt; web page&lt;/A&gt;. The EVK board includes the TJA1057GT/3.&lt;/P&gt;
&lt;P&gt;Details regarding the question can be found on Page 7 of this schematic.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;DIV id="tinyMceEditorGavin_Jia_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Feb 2026 02:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1020-EVK-FlexCAN-pin-mapping-and-CAN-hardware-availability/m-p/2322821#M36250</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2026-02-26T02:38:41Z</dc:date>
    </item>
  </channel>
</rss>