<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックDebugging IEE encrypted image for IMXRT1176</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-IEE-encrypted-image-for-IMXRT1176/m-p/2315416#M36166</link>
    <description>&lt;P&gt;I run an image which is encrypted using IEE. The image is mapped by my bootloader into the FLEXSPI IEE region and executes successfully. I'm wondering if it is possible to debug the code? If so any help or hint on how to do it would be appreciated. I'm using a Segger J-Link debugger.&lt;/P&gt;</description>
    <pubDate>Tue, 10 Feb 2026 09:30:19 GMT</pubDate>
    <dc:creator>tksec</dc:creator>
    <dc:date>2026-02-10T09:30:19Z</dc:date>
    <item>
      <title>Debugging IEE encrypted image for IMXRT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-IEE-encrypted-image-for-IMXRT1176/m-p/2315416#M36166</link>
      <description>&lt;P&gt;I run an image which is encrypted using IEE. The image is mapped by my bootloader into the FLEXSPI IEE region and executes successfully. I'm wondering if it is possible to debug the code? If so any help or hint on how to do it would be appreciated. I'm using a Segger J-Link debugger.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Feb 2026 09:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-IEE-encrypted-image-for-IMXRT1176/m-p/2315416#M36166</guid>
      <dc:creator>tksec</dc:creator>
      <dc:date>2026-02-10T09:30:19Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging IEE encrypted image for IMXRT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-IEE-encrypted-image-for-IMXRT1176/m-p/2318096#M36190</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229340"&gt;@tksec&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If the Encrypted XIP fuse has been blown, I'm afraid it is not possible to debug the code.&lt;/P&gt;
&lt;P&gt;As mentioned in the following community post.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-debug-after-ENCRYPT-XIP-EN-is-enabled/m-p/1481543" target="_blank"&gt;Re: How to debug after ENCRYPT_XIP_EN is enabled - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Fri, 13 Feb 2026 22:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-IEE-encrypted-image-for-IMXRT1176/m-p/2318096#M36190</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2026-02-13T22:40:39Z</dc:date>
    </item>
  </channel>
</rss>