<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-IMXRT1186 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FRDM-IMXRT1186/m-p/2314893#M36156</link>
    <description>&lt;P&gt;I want to &lt;U&gt;use&lt;/U&gt;&amp;nbsp;FRDM-IMXRT1186.&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;Application 1 &amp;gt;&lt;/STRONG&gt;&lt;/U&gt;&amp;nbsp;Board Should work with Internal 1.5MB RAM and with External QSPI Flash.&lt;/P&gt;&lt;P&gt;A&amp;gt; Ethernet 1 MII port (Named with Label ECAT0) can be configured with TCP/IP MODBUS Master ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;B&amp;gt; Ethernet 2 MII port (Named with Label ECAT1)&amp;nbsp;can be configured with ETHERCAT Master ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;U&gt;&lt;STRONG&gt;Application 2 &amp;gt;&lt;/STRONG&gt;&lt;/U&gt;&amp;nbsp;Board Should work with Internal 1.5MB RAM and with External QSPI Flash.&amp;nbsp;Arduino &amp;amp; MC Interface connector.&lt;/P&gt;&lt;P&gt;A&amp;gt; Ethernet 1 MII port (Named with Label ECAT0) &amp;amp; Ethernet 2 MII port (Named with Label ECAT1)&amp;nbsp;can be used for Ethercat Slave &amp;amp;&amp;nbsp;Arduino &amp;amp; MC Interface connector Analog/Digital GPIO ?&lt;/P&gt;</description>
    <pubDate>Mon, 09 Feb 2026 18:20:56 GMT</pubDate>
    <dc:creator>sarikaautomations</dc:creator>
    <dc:date>2026-02-09T18:20:56Z</dc:date>
    <item>
      <title>FRDM-IMXRT1186</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FRDM-IMXRT1186/m-p/2314893#M36156</link>
      <description>&lt;P&gt;I want to &lt;U&gt;use&lt;/U&gt;&amp;nbsp;FRDM-IMXRT1186.&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;Application 1 &amp;gt;&lt;/STRONG&gt;&lt;/U&gt;&amp;nbsp;Board Should work with Internal 1.5MB RAM and with External QSPI Flash.&lt;/P&gt;&lt;P&gt;A&amp;gt; Ethernet 1 MII port (Named with Label ECAT0) can be configured with TCP/IP MODBUS Master ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;B&amp;gt; Ethernet 2 MII port (Named with Label ECAT1)&amp;nbsp;can be configured with ETHERCAT Master ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;U&gt;&lt;STRONG&gt;Application 2 &amp;gt;&lt;/STRONG&gt;&lt;/U&gt;&amp;nbsp;Board Should work with Internal 1.5MB RAM and with External QSPI Flash.&amp;nbsp;Arduino &amp;amp; MC Interface connector.&lt;/P&gt;&lt;P&gt;A&amp;gt; Ethernet 1 MII port (Named with Label ECAT0) &amp;amp; Ethernet 2 MII port (Named with Label ECAT1)&amp;nbsp;can be used for Ethercat Slave &amp;amp;&amp;nbsp;Arduino &amp;amp; MC Interface connector Analog/Digital GPIO ?&lt;/P&gt;</description>
      <pubDate>Mon, 09 Feb 2026 18:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FRDM-IMXRT1186/m-p/2314893#M36156</guid>
      <dc:creator>sarikaautomations</dc:creator>
      <dc:date>2026-02-09T18:20:56Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-IMXRT1186</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FRDM-IMXRT1186/m-p/2322380#M36244</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259723"&gt;@sarikaautomations&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;&lt;SPAN&gt;A: It's recommend using J56A/J56B (RGMII ports for ETH0/ETH2) for TCP/IP/Modbus communication. Using J57A (ECAT0 port) is not advised.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;B: No. The RT1180 integrates ESC, not an ECAT master.&lt;/P&gt;
&lt;P&gt;2. Yes, this is supported.&lt;/P&gt;
&lt;P&gt;For more detailed information, please refer to this guide:&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/UM12450/page/topics/board_overview.html" target="_self"&gt;&lt;EM&gt;UM12450: FRDM-IMXRT1186 Board User Manual&lt;/EM&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Wed, 25 Feb 2026 08:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FRDM-IMXRT1186/m-p/2322380#M36244</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2026-02-25T08:41:33Z</dc:date>
    </item>
  </channel>
</rss>