<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1021 input max current in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1021-input-max-current/m-p/2296876#M36049</link>
    <description>&lt;P&gt;Hello, do you know how much current a GPIO input can handle? I'm using GPIO_AD_B1_02 and 8mA are flowing through that pin.&lt;/P&gt;&lt;P&gt;What is the maximum current an input can handle before damaging the pin?&lt;/P&gt;&lt;P&gt;The pin is on it's default values, if I understood right it is configured as input with 100k pulldown resistor by default&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jan 2026 21:13:18 GMT</pubDate>
    <dc:creator>jtrujillo</dc:creator>
    <dc:date>2026-01-20T21:13:18Z</dc:date>
    <item>
      <title>RT1021 input max current</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1021-input-max-current/m-p/2296876#M36049</link>
      <description>&lt;P&gt;Hello, do you know how much current a GPIO input can handle? I'm using GPIO_AD_B1_02 and 8mA are flowing through that pin.&lt;/P&gt;&lt;P&gt;What is the maximum current an input can handle before damaging the pin?&lt;/P&gt;&lt;P&gt;The pin is on it's default values, if I understood right it is configured as input with 100k pulldown resistor by default&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jan 2026 21:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1021-input-max-current/m-p/2296876#M36049</guid>
      <dc:creator>jtrujillo</dc:creator>
      <dc:date>2026-01-20T21:13:18Z</dc:date>
    </item>
    <item>
      <title>Re: RT1021 input max current</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1021-input-max-current/m-p/2297571#M36054</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258966"&gt;@jtrujillo&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In general, the maximum current for any RT1xxx GPIO pin should be limited to 25mA whether it is sourcing or sinking current. This is the safe limit for the technology to prevent reliability issues, like latent damage due to electromigration, and can be sustained for long durations if the pin needs to.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jan 2026 18:49:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1021-input-max-current/m-p/2297571#M36054</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2026-01-21T18:49:44Z</dc:date>
    </item>
  </channel>
</rss>