<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT1170-EVKB: Continuous Reset in Non-Debug Mode When Using ROMAPI in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVKB-Continuous-Reset-in-Non-Debug-Mode-When-Using/m-p/2265511#M35898</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258131"&gt;@passman&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If you debug an SDK example, such as hello_world_cm7 without modifications, does the same issue occur?&lt;/P&gt;
&lt;P&gt;Also, the SDK (version 26.09) provides an example in Keil for using the ROM_API called "fsl_romapi_cm7", which could be helpful.&lt;BR /&gt;Additionally, Chapter 10.13, called "ROM APIs", offers detailed information and code examples for its usage.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
    <pubDate>Wed, 17 Dec 2025 22:31:36 GMT</pubDate>
    <dc:creator>Habib_MS</dc:creator>
    <dc:date>2025-12-17T22:31:36Z</dc:date>
    <item>
      <title>MIMXRT1170-EVKB: Continuous Reset in Non-Debug Mode When Using ROMAPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVKB-Continuous-Reset-in-Non-Debug-Mode-When-Using/m-p/2264984#M35893</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I am working with the MIMXRT1170-EVKB development board. I cloned a &lt;/SPAN&gt;hello_world_cm7&lt;SPAN&gt; project and integrated the ROM API demo code into it. While debugging, the output shows successful execution, but when running in non-debug mode, the board continuously resets and fails to operate normally. Are any additional modifications required?&lt;/SPAN&gt;&lt;/P&gt;&lt;HR /&gt;&lt;P class=""&gt;&lt;SPAN&gt;Configuration Tool: MCUXpresso Config Tools 25.09&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SDK: SDK_25_09_00_MIMXRT1170-EVKB&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Keil MDK: 5.43.1.0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Keil MDK Project: flexspi_nor_debug&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 12:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVKB-Continuous-Reset-in-Non-Debug-Mode-When-Using/m-p/2264984#M35893</guid>
      <dc:creator>passman</dc:creator>
      <dc:date>2025-12-17T12:05:55Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVKB: Continuous Reset in Non-Debug Mode When Using ROMAPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVKB-Continuous-Reset-in-Non-Debug-Mode-When-Using/m-p/2265511#M35898</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258131"&gt;@passman&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If you debug an SDK example, such as hello_world_cm7 without modifications, does the same issue occur?&lt;/P&gt;
&lt;P&gt;Also, the SDK (version 26.09) provides an example in Keil for using the ROM_API called "fsl_romapi_cm7", which could be helpful.&lt;BR /&gt;Additionally, Chapter 10.13, called "ROM APIs", offers detailed information and code examples for its usage.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 22:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVKB-Continuous-Reset-in-Non-Debug-Mode-When-Using/m-p/2265511#M35898</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-12-17T22:31:36Z</dc:date>
    </item>
  </channel>
</rss>