<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: getting started with rt1062 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/getting-started-with-rt1062/m-p/2248748#M35724</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256190"&gt;@yacineykr&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;There is not a specific guide for starting a project from scratch, but you can use the SDK examples as a reference to understand how the peripherals work and how they are configured.&lt;BR /&gt;Additionally, the SDK (version 25.09) provides examples that demonstrate how to use CMSIS drivers with certain peripherals, as shown in the following image:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Habib_MS_0-1764120216601.png" style="width: 620px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367207i63DDBDEC0ABC1E34/image-dimensions/620x199?v=v2" width="620" height="199" role="button" title="Habib_MS_0-1764120216601.png" alt="Habib_MS_0-1764120216601.png" /&gt;&lt;/span&gt;&lt;BR /&gt;On the other hand, CMSIS drivers can be used either with interrupts or DMA, depending on the configurations you apply. I highly recommend using the SDK examples as a reference when developing your application.&lt;BR /&gt;Finally, there are no examples that are strictly bare metal, but as I mentioned, you can refer to the SDK examples and those available in the &lt;A href="https://mcuxpresso.nxp.com/appcodehub" target="_self"&gt;Application Code Hub&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
    <pubDate>Wed, 26 Nov 2025 01:24:44 GMT</pubDate>
    <dc:creator>Habib_MS</dc:creator>
    <dc:date>2025-11-26T01:24:44Z</dc:date>
    <item>
      <title>getting started with rt1062</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/getting-started-with-rt1062/m-p/2206728#M35683</link>
      <description>&lt;P&gt;I am new to the NXP ecosystem and I’m struggling to find my way around it.&lt;/P&gt;&lt;P&gt;I have a custom board based on the &lt;STRONG&gt;RT1062 MCU&lt;/STRONG&gt;, and I’m using &lt;STRONG&gt;MCUXpresso IDE&lt;/STRONG&gt; with the &lt;STRONG&gt;MCU SDK (not the evaluation board SDK)&lt;/STRONG&gt;.&lt;BR /&gt;I tried creating a project in the IDE, then adding the &lt;STRONG&gt;CMSIS UART drivers&lt;/STRONG&gt; to test a simple UART transmit function. Since I couldn’t get XIP to work yet on my external flash, I linked the project to &lt;STRONG&gt;run from RAM&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;The project builds the first time without any issues.&lt;BR /&gt;However, once I open &lt;STRONG&gt;MCUXpresso Config Tools&lt;/STRONG&gt; to configure the UART peripheral and rebuild, the project reports missing drivers.&lt;BR /&gt;I tried adding them again through SDK Management in Project Properties, but the problem persists.&lt;/P&gt;&lt;P&gt;So my questions are:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Do you have any recommendations or best practices for setting up a project for a custom RT1062 board, especially for boot configuration and ensuring that basic peripherals compile correctly?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Do CMSIS UART drivers require DMA to be enabled?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there a simple way to write bare-metal tests for peripherals (UART, I2C, SPI) using only the MCUXpresso IDE, without the need for DMA or higher-level frameworks?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Nov 2025 10:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/getting-started-with-rt1062/m-p/2206728#M35683</guid>
      <dc:creator>yacineykr</dc:creator>
      <dc:date>2025-11-18T10:05:31Z</dc:date>
    </item>
    <item>
      <title>Re: getting started with rt1062</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/getting-started-with-rt1062/m-p/2248748#M35724</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256190"&gt;@yacineykr&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;There is not a specific guide for starting a project from scratch, but you can use the SDK examples as a reference to understand how the peripherals work and how they are configured.&lt;BR /&gt;Additionally, the SDK (version 25.09) provides examples that demonstrate how to use CMSIS drivers with certain peripherals, as shown in the following image:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Habib_MS_0-1764120216601.png" style="width: 620px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367207i63DDBDEC0ABC1E34/image-dimensions/620x199?v=v2" width="620" height="199" role="button" title="Habib_MS_0-1764120216601.png" alt="Habib_MS_0-1764120216601.png" /&gt;&lt;/span&gt;&lt;BR /&gt;On the other hand, CMSIS drivers can be used either with interrupts or DMA, depending on the configurations you apply. I highly recommend using the SDK examples as a reference when developing your application.&lt;BR /&gt;Finally, there are no examples that are strictly bare metal, but as I mentioned, you can refer to the SDK examples and those available in the &lt;A href="https://mcuxpresso.nxp.com/appcodehub" target="_self"&gt;Application Code Hub&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 01:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/getting-started-with-rt1062/m-p/2248748#M35724</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-11-26T01:24:44Z</dc:date>
    </item>
  </channel>
</rss>