<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Quadrature Encoder Velocity Measurement</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-Velocity-Measurement/m-p/2195531#M35525</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you I have made a support case with the same title as this one.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 30 Oct 2025 06:33:32 GMT</pubDate>
    <dc:creator>RegulaTor</dc:creator>
    <dc:date>2025-10-30T06:33:32Z</dc:date>
    <item>
      <title>Quadrature Encoder Velocity Measurement</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-Velocity-Measurement/m-p/2194405#M35502</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to figure out how to use a timer to improve low speed quadrature encoder measurements on i.MX RT1060. I can see in the reference manual (55.4.2 Prescaler for Slow or Fast Speed Measurement) that there should be some support for low speed measurements using a timer. However, I am having a hard time understanding how I can set this up? Are the some examples since &lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-speed-measurement/m-p/1681289" target="_self"&gt;this was posted&lt;/A&gt;?&lt;/P&gt;&lt;P&gt;If not could you provide a brief explanation of what I need to do? Does the ENC have its own timer or should I setup a separate timer?&amp;nbsp; What are the steps for setting up such a timer?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tor&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 15:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-Velocity-Measurement/m-p/2194405#M35502</guid>
      <dc:creator>RegulaTor</dc:creator>
      <dc:date>2025-10-28T15:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Encoder Velocity Measurement</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-Velocity-Measurement/m-p/2194974#M35507</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256251"&gt;@RegulaTor&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, we have such kind of demo but it is just internal used, would you please raise a private case for it? Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO" target="_blank"&gt;https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 08:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-Velocity-Measurement/m-p/2194974#M35507</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-10-29T08:46:34Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Encoder Velocity Measurement</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-Velocity-Measurement/m-p/2195531#M35525</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you I have made a support case with the same title as this one.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 06:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Quadrature-Encoder-Velocity-Measurement/m-p/2195531#M35525</guid>
      <dc:creator>RegulaTor</dc:creator>
      <dc:date>2025-10-30T06:33:32Z</dc:date>
    </item>
  </channel>
</rss>