<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Dual Core using the same peripherals in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2194258#M35500</link>
    <description>&lt;P&gt;thank you for your answer.&lt;BR /&gt;You mean I can configure&amp;nbsp;&lt;SPAN&gt;on separate cores without the same peripherals?&lt;BR /&gt;I need to share 1024 bytes data from CM4 to CM7. Should I use MU, SEMA4 or Free-RTOS Message Buffers for this application for best performance?&amp;nbsp;&lt;BR /&gt;If using Free-RTOS how can I config receive data via IRS RTOS?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 28 Oct 2025 10:39:28 GMT</pubDate>
    <dc:creator>nampt</dc:creator>
    <dc:date>2025-10-28T10:39:28Z</dc:date>
    <item>
      <title>Dual Core using the same peripherals</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2193844#M35486</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;"I am using the MIMXRT1170 and building a dual-core project with MCUXpresso Config and IAR Workbench.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I'm wondering how to create the project. Should I configure, generate all peripherals in the master core (CM7) or on separate cores? And what should I do if both cores are using the same peripherals?"&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;&lt;LI-PRODUCT title="MIMXRT1170-EVK" id="MIMXRT1170-EVK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 02:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2193844#M35486</guid>
      <dc:creator>nampt</dc:creator>
      <dc:date>2025-10-28T02:29:07Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Core using the same peripherals</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2194209#M35495</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239761"&gt;@nampt&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Please refer to this application note, it is very helpful.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13264.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13264.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Question1:&amp;nbsp;&lt;SPAN&gt;I'm wondering how to create the project. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Answer1:&amp;nbsp; For MCUXPresso IDE, you can import SDK demo as the following Fig show.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_0-1761643982096.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/362860i1DF1A224D8993658/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_0-1761643982096.png" alt="mayliu1_0-1761643982096.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For IAR.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_1-1761644634804.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/362869i1240B6A174EF5638/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_1-1761644634804.png" alt="mayliu1_1-1761644634804.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Question2:&amp;nbsp; S&lt;SPAN&gt;hould I configure, generate all peripherals in the master core (CM7) or on separate cores? And what should I do if both cores are using the same peripherals?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Answer2:&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Please note that multi-core&amp;nbsp;can not using the&amp;nbsp;same peripherals at same time.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please refer to the&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13264.pdf" target="_blank"&gt;AN13264&lt;/A&gt;&amp;nbsp;and&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13114.pdf" target="_blank"&gt;AN13114&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps you.&lt;BR /&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 09:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2194209#M35495</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-10-28T09:46:31Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Core using the same peripherals</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2194258#M35500</link>
      <description>&lt;P&gt;thank you for your answer.&lt;BR /&gt;You mean I can configure&amp;nbsp;&lt;SPAN&gt;on separate cores without the same peripherals?&lt;BR /&gt;I need to share 1024 bytes data from CM4 to CM7. Should I use MU, SEMA4 or Free-RTOS Message Buffers for this application for best performance?&amp;nbsp;&lt;BR /&gt;If using Free-RTOS how can I config receive data via IRS RTOS?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 10:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2194258#M35500</guid>
      <dc:creator>nampt</dc:creator>
      <dc:date>2025-10-28T10:39:28Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Core using the same peripherals</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2194981#M35508</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239761"&gt;@nampt&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I think you can&amp;nbsp; refer to the SDK demo shown in below Fig.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_0-1761727927639.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/363062iC00685D89CFF21F2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_0-1761727927639.png" alt="mayliu1_0-1761727927639.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_1-1761728029038.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/363063i04B53510349DF1FF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_1-1761728029038.png" alt="mayliu1_1-1761728029038.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 08:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2194981#M35508</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-10-29T08:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Core using the same peripherals</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2302548#M36105</link>
      <description>Many thanks!</description>
      <pubDate>Thu, 29 Jan 2026 03:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Dual-Core-using-the-same-peripherals/m-p/2302548#M36105</guid>
      <dc:creator>nampt</dc:creator>
      <dc:date>2026-01-29T03:14:49Z</dc:date>
    </item>
  </channel>
</rss>