<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Boot from SD Card</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2189677#M35451</link>
    <description>Thank you, it is a great help.</description>
    <pubDate>Tue, 21 Oct 2025 06:57:54 GMT</pubDate>
    <dc:creator>abady1000</dc:creator>
    <dc:date>2025-10-21T06:57:54Z</dc:date>
    <item>
      <title>Boot from SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2136839#M34758</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I use NXP RT1170, my application is big, I use almost the whole OC RAM (OC1 + OC2 + ECC1 + ECC2), I sue also the other RAM Segments (DTC, ITC, SDRAM)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My application is linked to RAM, and when I upload application it uploads every segment into the correct palce it should be in.&lt;BR /&gt;&lt;BR /&gt;I want now to build a bootable image form SD Card, how to do so?&lt;BR /&gt;&lt;BR /&gt;My idea is to modify linker script manually and make all sections uploaded to SDRAM, then in boot CPU put every section in its correct place using Linker Load/Execute address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this doable? is there other better means to achieve this?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;BTW, when I use Secure Provisioning tool I get this error message after selecting my axf file:&lt;BR /&gt;ERROR: The selected image size 540234688 is greater than the selected boot memory size 67108864.&lt;/P&gt;</description>
      <pubDate>Sat, 19 Jul 2025 09:30:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2136839#M34758</guid>
      <dc:creator>abady1000</dc:creator>
      <dc:date>2025-07-19T09:30:39Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2137074#M34768</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236627"&gt;@abady1000&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;I suggest you can refer to this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT1050-SDRAM-app-code-boot-from-SDcard-burn-with-3-tools/ta-p/1129008" target="_blank"&gt;RT1050 SDRAM app code boot from SDcard burn with 3 tools - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;This document is about the RT series app running on the external SDRAM, but boot from SD card.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps you.&lt;BR /&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Wish you a nice day!&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jul 2025 06:23:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2137074#M34768</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-07-21T06:23:56Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2189677#M35451</link>
      <description>Thank you, it is a great help.</description>
      <pubDate>Tue, 21 Oct 2025 06:57:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2189677#M35451</guid>
      <dc:creator>abady1000</dc:creator>
      <dc:date>2025-10-21T06:57:54Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2190466#M35457</link>
      <description>&lt;P&gt;You are welcome, and thanks for your reply.&lt;/P&gt;
&lt;P&gt;If this post answers your question, please accept it as&amp;nbsp; solution.&lt;/P&gt;
&lt;P&gt;If you meet any issue in the future, welcome to create the new question post.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Oct 2025 06:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-SD-Card/m-p/2190466#M35457</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-10-22T06:22:08Z</dc:date>
    </item>
  </channel>
</rss>