<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NXP RT1170 Output Voltage level in Parallel output in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/NXP-RT1170-Output-Voltage-level-in-Parallel-output/m-p/2187340#M35439</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236627"&gt;@abady1000&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;1：Please confirm that the IO bank used for the parallel interface is powered by 3.3V. Measure the voltage using an oscilloscope and provide screenshots of the relevant module schematic design.&amp;nbsp;Have you compared the hardware design of your custom development board with that of the MIMXRT1170-EVKB?&lt;/P&gt;
&lt;P&gt;2: Please confirm that the program running on the MIMXRT1170-EVKB development board without issues is completely identical to the program running on your custom development board.&lt;/P&gt;
&lt;P&gt;3: Have you tried reducing the clock frequency to see if the occurrence of the anomaly decreases?&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;MayLiu&lt;/P&gt;</description>
    <pubDate>Thu, 16 Oct 2025 10:51:46 GMT</pubDate>
    <dc:creator>mayliu1</dc:creator>
    <dc:date>2025-10-16T10:51:46Z</dc:date>
    <item>
      <title>NXP RT1170 Output Voltage level in Parallel output</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/NXP-RT1170-Output-Voltage-level-in-Parallel-output/m-p/2186445#M35428</link>
      <description>&lt;P&gt;I have a problem in a custom board, the is in voltage level in the clock generated from NXP RT1176 parallel interface !&lt;/P&gt;&lt;P&gt;I have manufactured a board based on chip NXP RT1170, I received the board and it worked well with me, and every thing seems fine.&lt;/P&gt;&lt;P&gt;I started developing on the MCU, I was able to receive BT656 video using CSI, I was able to use its parallel interface and stream video to micro display and I was able to use multiple different serial interfaces successfully.&lt;/P&gt;&lt;P&gt;I noticed random red dots appear on the display, they are very clear when the video is Black&amp;amp;White, I did a lot of investigation on this issue but couldn't find the cause. I checked all frame buffers inside RAM (SDR) but they all are fine!&lt;/P&gt;&lt;P&gt;I measured RGB parallel signals (when sending B&amp;amp;W, they all should be the same) and they seems identical, no differences in rising time or falling time, they all behave the same. I also changed the boards, wires, micro displays, but nothing changed.&lt;/P&gt;&lt;P&gt;One thing I noticed was the Parallel output clock was a little bit out of the level it should be on!&lt;/P&gt;&lt;P&gt;The clock frequency is correct, but voltage level is (-0.7V , 3.9V) instead of (0V, 3.3V)!&lt;/P&gt;&lt;P&gt;I am not sure if this is what causing the issue, but is this level correct?! (it is obviously not), what could cause the issue?&lt;/P&gt;&lt;P&gt;I checked all the input voltage to the system and their level is correct.&lt;/P&gt;&lt;P&gt;I ran the same application in the evaluation board EVKB-MIMXRT1170 and the level is good!&lt;/P&gt;&lt;P&gt;My chip exact number is "MIMXRT1176CVM8A" and the evaluations chip exact number is "MIMXRT1176DVMAA"&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 08:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/NXP-RT1170-Output-Voltage-level-in-Parallel-output/m-p/2186445#M35428</guid>
      <dc:creator>abady1000</dc:creator>
      <dc:date>2025-10-15T08:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: NXP RT1170 Output Voltage level in Parallel output</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/NXP-RT1170-Output-Voltage-level-in-Parallel-output/m-p/2187340#M35439</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236627"&gt;@abady1000&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;1：Please confirm that the IO bank used for the parallel interface is powered by 3.3V. Measure the voltage using an oscilloscope and provide screenshots of the relevant module schematic design.&amp;nbsp;Have you compared the hardware design of your custom development board with that of the MIMXRT1170-EVKB?&lt;/P&gt;
&lt;P&gt;2: Please confirm that the program running on the MIMXRT1170-EVKB development board without issues is completely identical to the program running on your custom development board.&lt;/P&gt;
&lt;P&gt;3: Have you tried reducing the clock frequency to see if the occurrence of the anomaly decreases?&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 10:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/NXP-RT1170-Output-Voltage-level-in-Parallel-output/m-p/2187340#M35439</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-10-16T10:51:46Z</dc:date>
    </item>
    <item>
      <title>Re: NXP RT1170 Output Voltage level in Parallel output</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/NXP-RT1170-Output-Voltage-level-in-Parallel-output/m-p/2189694#M35452</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;&amp;nbsp;for your response.&lt;BR /&gt;&lt;BR /&gt;1: I will return for this point once I prepare the measures for you.&lt;BR /&gt;&lt;BR /&gt;2: Yes, it was exactly the same, I didn't change even a comment, I uploaded the same exact binary on both boards, I didn't even change the IOs.&lt;BR /&gt;&lt;BR /&gt;3: I tried both increasing and decreasing the clock speed, and it seems that is irrelevant to the issue, nothing changed.&lt;BR /&gt;My original clock speed is (~37.5MHz), I tried both (~70.0 MHz) and (~15.0 MHz) and there were no change in the behavior of the clock.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 07:09:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/NXP-RT1170-Output-Voltage-level-in-Parallel-output/m-p/2189694#M35452</guid>
      <dc:creator>abady1000</dc:creator>
      <dc:date>2025-10-21T07:09:29Z</dc:date>
    </item>
  </channel>
</rss>