<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Octal flash IS25WX256 dummy cycles in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octal-flash-IS25WX256-dummy-cycles/m-p/2178983#M35352</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I have some trouble understanding how to specify the correct number of dummy cycles for the Octal Read command. According to the flash datasheet, it defaults to 16 and the maximum supported frequency is 162 MHz for Octal I/O fast read:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tbonkers_2-1759348696539.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359227iF1573B6B6441EF61/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tbonkers_2-1759348696539.png" alt="tbonkers_2-1759348696539.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tbonkers_0-1759348608697.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359225i993B0FDF7E076682/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tbonkers_0-1759348608697.png" alt="tbonkers_0-1759348608697.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Based on the requirement for 16 dummy cycles for DDR read command, and my FlexSPI clock being 80 MHz, what is the number I need to use as an argument for the&amp;nbsp;DUMMY_DDR command?&lt;/P&gt;&lt;P&gt;I pointed out that the FCB created by NXP Secure Provisioning Tool uses 6 dummy cycles at 80 MHz clock - is that the correct value?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 01 Oct 2025 20:05:56 GMT</pubDate>
    <dc:creator>tbonkers</dc:creator>
    <dc:date>2025-10-01T20:05:56Z</dc:date>
    <item>
      <title>Octal flash IS25WX256 dummy cycles</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octal-flash-IS25WX256-dummy-cycles/m-p/2178828#M35347</link>
      <description>&lt;P&gt;I am trying to interface MIMXRT1166 with octal flash &lt;A href="https://www.issi.com/WW/pdf/25LX-WX256-128.pdf" target="_self"&gt;IS25WX256&lt;/A&gt;, and I'm not sure about the correct setting of dummy cycles for the 0xFD (4-BYTE DDR OCTAL I/O FAST READ with DDR ADDRESS and DATA) command.&lt;/P&gt;&lt;P&gt;The FCB generated by MCUXpresso Secure Provisioning Tool uses 6 dummy cycles, whereas the flash datasheet specifies 16 dummy cycles as default. Both of these settings result in the board crashing after some time. I've tried different clocks and combinations of dummy cycles, all of which end up in a crash after a few minutes or an hour.&lt;/P&gt;&lt;P&gt;The FCB code is below:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;/* Default dummy cycles for 0xFD read command. Max freq. of 162 MHz in Octal DDR mode */
#define DUMMY_CYCLES 16

const flexspi_nor_config_t
	issi_flash_config =
		{
			.memConfig =
				{
					.tag = (0x42464346UL),
					.version = (0x56010400UL),
					.reserved0 = 0,
					.readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
					.csHoldTime = 3,
					.csSetupTime = 3,
					.columnAddressWidth = 0,
					.deviceModeCfgEnable = 1, /* Device mode command enabled */
					.deviceModeType = kDeviceConfigCmdType_Spi2Xpi,
					.waitTimeCfgCommands = 1, /* If not zero, flexspi will wait instead of read status */
					.deviceModeSeq =
						{
							.seqNum = 1U,
							.seqId = 6U,
							.reserved = 0U,
						},
					/* Only effective when deviceModeCfgEnable = 1 */
					.deviceModeArg = 0xE7,
					/* Enable flash configuration feature */
					.configCmdEnable = 0,
					.configModeType[0] = kDeviceConfigCmdType_Generic,
					.configModeType[1] = kDeviceConfigCmdType_Generic,
					.configModeType[2] = kDeviceConfigCmdType_Generic,

					.configCmdSeqs[0] = {.seqNum = 1U, .seqId = 13U, .reserved = 0U}, /* cmd seq 0 Set dummy cycles */
					.configCmdSeqs[1] = {.seqNum = 1U, .seqId = 10U, .reserved = 0U}, /* cmd seq 1 Enable XIP */
					.configCmdSeqs[2] = {.seqNum = 1U, .seqId = 7U, .reserved = 0U},  /* cmd seq 2 Enable 4-byte addressing */

					.reserved1 = 0,
					.configCmdArgs[0] = DUMMY_CYCLES, /* Argument for cmd seq 0 */
					.configCmdArgs[1] = 0xFE,         /* Argument for cmd seq 1 */
					.configCmdArgs[2] = 0xFE,         /* Argument for cmd seq 2 */

					.reserved2 = 0,
					/* Do not override pad settings with the Misc option */
					.controllerMiscOption =
						0x00 | (1u &amp;lt;&amp;lt; kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u &amp;lt;&amp;lt; kFlexSpiMiscOffset_DdrModeEnable),
					.deviceType = kFlexSpiDeviceType_SerialNOR,
					.sflashPadType = 8,
					.serialClkFreq = kFlexSpiSerialClk_80MHz, /* Note DDR frequency is double that figure */
					.lutCustomSeqEnable = 0,
					.reserved3[0] = 0,
					.reserved3[1] = 0,
					.sflashA1Size = 32 * 1024 * 1024,
					.sflashA2Size = 0,
					.sflashB1Size = 0,
					.sflashB2Size = 0,
					.csPadSettingOverride = 0xA, /* Pulldown enabled, normal drive strength */
					.sclkPadSettingOverride = 0xA,
					.dataPadSettingOverride = 0xA,
					.dqsPadSettingOverride = 0xA,
					.timeoutInMs = 0,
					.commandInterval = 10,
					.dataValidTime[0] = 16,
					.dataValidTime[1] = 16,
					.busyOffset = 0,
					.busyBitPolarity = 0,
					.lookupTable =
						{
							/* LUT table discussed at p. 297 of the RM */

							/* [0] DDR OCTAL I/O FAST READ FDh  */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 0xFD, RADDR_DDR, FLEXSPI_8PAD, 32),
							FLEXSPI_LUT_SEQ(DUMMY_DDR, FLEXSPI_8PAD, DUMMY_CYCLES, READ_DDR, FLEXSPI_8PAD, 4),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [1] Read Status Register - SPI */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 4),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [2] Read Status Register in octal mode*/
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 0x05, DUMMY_DDR, FLEXSPI_8PAD, DUMMY_CYCLES),
							FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 1, STOP, FLEXSPI_1PAD, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [3] Write Enable */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [4] Write Enable Octal */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 6, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [5] Erase Sector */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 33, RADDR_DDR, FLEXSPI_8PAD, 32),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [6] Write volatile configuration register for entering octal mode */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x81, CMD_SDR, FLEXSPI_1PAD, 0),
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0, CMD_SDR, FLEXSPI_1PAD, 0),
							FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 1, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [7]  Write NVREG at address 6 to enable 4-byte addr
							 */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x81, CMD_SDR, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, CMD_SDR, FLEXSPI_1PAD, 0x05),
							FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x01, STOP, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [8] 4-BYTE 128KB SECTOR ERASE */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 220, RADDR_DDR, FLEXSPI_8PAD, 32),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [9] Page Program 4 byte */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 18, RADDR_DDR, FLEXSPI_8PAD, 32),
							FLEXSPI_LUT_SEQ(WRITE_DDR, FLEXSPI_8PAD, 4, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [10]  Write NVREG at address 6 to enable XIP - SPI */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x81, CMD_SDR, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, CMD_SDR, FLEXSPI_1PAD, 0x06),
							FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x01, STOP, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [11] Chip Erase */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 96, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [12] Write NVREG at address 1 to set dummy cycles in octal mode */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 0x81, CMD_DDR, FLEXSPI_8PAD, 0x00),
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_8PAD, 0x00, CMD_DDR, FLEXSPI_8PAD, 0x01),
							FLEXSPI_LUT_SEQ(WRITE_DDR, FLEXSPI_8PAD, 0x01, STOP, FLEXSPI_8PAD, 0x00),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [13]  Write NVREG at address 1 to set the dummy cycles - SPI */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x81, CMD_SDR, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, CMD_SDR, FLEXSPI_1PAD, 0x01),
							FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x01, STOP, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* (14) Write NVREG at address 0 to switch to chosen
							   interface-Type - SPI */
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x81, CMD_SDR, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, CMD_SDR, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x01, STOP, FLEXSPI_1PAD, 0x00),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

							/* [15] Dummy command */
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),
							FLEXSPI_LUT_SEQ(0, 0, 0, 0, 0, 0),

						},
				},
			.pageSize = 256,
			.sectorSize = 4096,
			.ipcmdSerialClkFreq = 1, /* 30 MHz for IP commands */
			.isUniformBlockSize = 0,
			.reserved0 = 0,
			.serialNorType = 2,
			.needExitNoCmdMode = 0,
			.halfClkForNonReadCmd = 0,
			.needRestoreNoCmdMode = 0,
			.blockSize = 128 * 1024,
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Oct 2025 13:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octal-flash-IS25WX256-dummy-cycles/m-p/2178828#M35347</guid>
      <dc:creator>tbonkers</dc:creator>
      <dc:date>2025-10-01T13:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: Octal flash IS25WX256 dummy cycles</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octal-flash-IS25WX256-dummy-cycles/m-p/2178944#M35349</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183978"&gt;@tbonkers&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please refer to the FCB file of the following knowledge base article:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT1170-Octal-flash-enablement/ta-p/1498369" target="_blank"&gt;RT1170 Octal flash enablement - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 01 Oct 2025 18:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octal-flash-IS25WX256-dummy-cycles/m-p/2178944#M35349</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-10-01T18:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: Octal flash IS25WX256 dummy cycles</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octal-flash-IS25WX256-dummy-cycles/m-p/2178983#M35352</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I have some trouble understanding how to specify the correct number of dummy cycles for the Octal Read command. According to the flash datasheet, it defaults to 16 and the maximum supported frequency is 162 MHz for Octal I/O fast read:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tbonkers_2-1759348696539.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359227iF1573B6B6441EF61/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tbonkers_2-1759348696539.png" alt="tbonkers_2-1759348696539.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tbonkers_0-1759348608697.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359225i993B0FDF7E076682/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tbonkers_0-1759348608697.png" alt="tbonkers_0-1759348608697.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Based on the requirement for 16 dummy cycles for DDR read command, and my FlexSPI clock being 80 MHz, what is the number I need to use as an argument for the&amp;nbsp;DUMMY_DDR command?&lt;/P&gt;&lt;P&gt;I pointed out that the FCB created by NXP Secure Provisioning Tool uses 6 dummy cycles at 80 MHz clock - is that the correct value?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 01 Oct 2025 20:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octal-flash-IS25WX256-dummy-cycles/m-p/2178983#M35352</guid>
      <dc:creator>tbonkers</dc:creator>
      <dc:date>2025-10-01T20:05:56Z</dc:date>
    </item>
  </channel>
</rss>