<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックIMXRT1176 HAB Authentication Status</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-HAB-Authentication-Status/m-p/2151191#M34947</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We're using signed images on the IMXRT1176. Right now the device is in open mode because we'd like to confirm the HAB is authenticating the image before closing the device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is that the ROM has an API that can return the status of the authentication. After looking into it a bit, it looks like it's not available on this device. All I see are functions for the flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any other way I can read the status?&lt;/P&gt;</description>
    <pubDate>Tue, 12 Aug 2025 23:52:11 GMT</pubDate>
    <dc:creator>rnicolls</dc:creator>
    <dc:date>2025-08-12T23:52:11Z</dc:date>
    <item>
      <title>IMXRT1176 HAB Authentication Status</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-HAB-Authentication-Status/m-p/2151191#M34947</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We're using signed images on the IMXRT1176. Right now the device is in open mode because we'd like to confirm the HAB is authenticating the image before closing the device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is that the ROM has an API that can return the status of the authentication. After looking into it a bit, it looks like it's not available on this device. All I see are functions for the flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any other way I can read the status?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 23:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-HAB-Authentication-Status/m-p/2151191#M34947</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2025-08-12T23:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1176 HAB Authentication Status</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-HAB-Authentication-Status/m-p/2152233#M34959</link>
      <description>&lt;P&gt;Would you please use SEC or MCUBootUtility tool to check if HAB enabled or not?&amp;nbsp;&lt;A href="https://docs.mcuxpresso.nxp.com/secure/latest/06_processor_specific_workflow.html#booting-encrypted-hab-authenticated-image" target="_blank"&gt;https://docs.mcuxpresso.nxp.com/secure/latest/06_processor_specific_workflow.html#booting-encrypted-hab-authenticated-image&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Aug 2025 08:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-HAB-Authentication-Status/m-p/2152233#M34959</guid>
      <dc:creator>Sam_Gao</dc:creator>
      <dc:date>2025-08-14T08:57:21Z</dc:date>
    </item>
  </channel>
</rss>